Other Parts Discussed in Thread: OMAP-L138
Hi,
We have designed a custom board using c6748 processor.
For booting of SPI flash We use OMAP-L138_FlashAndBootUtils_2_40.
The problem is that when i run the utility sfh_OMAP-L138.exe in command line then it will stop at [ "Waiting for SFT on the OMAP-L138..." and nothing happens. ].
The command i use is sfh_OMAP-L138.exe -erase -targetType C6748.
This command is working fine on my logic pd kit but dont work on my custom board.
So any suggestions in this problem.
Umar