Hello,
I am very new in ARM development, and I cannot find precise information about the following points before buying the ICE board. I am sorry if my questions are a bit stupid, but maybe you can help me :
- What exactly contains the ICE 3359 kit sold by TI ? Does it provides power supply and cables ? Some descriptions seem yes, others seem it is just the board which is sold.
- In the same way, does Code Composer provided in the kit (even in demo version) or do I need to buy it separately ?
- I would like to have a RS232 interface. I know that the ICE doesn’t have a RS232, but has an UART output (and I can add a RS232 transceiver). However it is written in the specification that this UART is exclusively for debug… Did I miss something, or there is really no way to do that ?
- I would like to buy the ICE for 2 different project. However, one needs an EtherCAT interface (provided buy ICE), but the over needs a simple Ethernet interface. I read in some forums that Ethernet is not supported buy ICE and that it is difficult to setup, but in the examples provided buy SYS/BIOS it seems that it is what enetLwip does, am I wrong ?
Thank you in advance,
Paul.