Hi,
I am trying to implement the edma example given in "...\ti\pdk_C6678_1_1_2_5\packages\ti\csl\example\edma" on c6678 DSP. From my understanding of EDMA, after the transfer is complete, the dstBuff must have the same data as that of srcBuff but when i am printing the data i dont see that as the case. The code i have implemented(Modified the original example slightly) is as below:
#include <stdio.h>
#include <ti/csl/csl_edma3.h>
#include <ti/csl/csl_edma3Aux.h>
#include <ti/csl/csl_cacheAux.h>
/**********************************************************************
************************** Global Variables **************************
**********************************************************************/
/* Global Variables which are used to dump the TPCC register overlay in the
* debugger... */
//CSL_TpccRegs* gEDMACC0Regs = (CSL_TpccRegs*)CSL_EDMA0CC_REGS;
//CSL_TpccRegs* gEDMACC1Regs = (CSL_TpccRegs*)CSL_EDMA1CC_REGS;
CSL_TpccRegs* gEDMACC2Regs = (CSL_TpccRegs*)CSL_EDMA2CC_REGS;
/* Global Buffers (Source and Destination) for PING-PONG */
Uint8 srcBuff1[512];
Uint8 srcBuff2[512];
Uint8 dstBuff1[512];
Uint8 dstBuff2[512];
void print()
{
int i;
for(i=0;i<256;i++)
printf("%u %u %u %u\n",srcBuff1[i],srcBuff2[i],dstBuff1[i],dstBuff2[i]);
}
static Bool Verify_Transfer
(
Uint16 aCnt,
Uint16 bCnt,
Uint16 cCnt,
Uint16 srcBIdx,
Uint16 dstBIdx,
Uint16 srcCIdx,
Uint16 dstCIdx,
Uint8 *srcBuff,
Uint8 *dstBuff,
Bool abSync
)
{
Uint32 loopIndex1;
Uint32 loopIndex2;
Uint32 loopIndex3;
Uint8* srcArrayPtr = (Uint8*)srcBuff;
Uint8* dstArrayPtr = (Uint8*)dstBuff;
Uint8* srcFramePtr = (Uint8*)srcBuff;
Uint8* dstFramePtr = (Uint8*)dstBuff;
Uint16 key;
/* Invalidate the cache before verification */
/* Disable Interrupts */
key = _disable_interrupts();
CACHE_invL1d ((void *)srcBuff, 512, CACHE_WAIT);
CACHE_invL2 ((void *)srcBuff, 512, CACHE_WAIT);
CACHE_invL1d ((void *)dstBuff, 512, CACHE_WAIT);
CACHE_invL2 ((void *)dstBuff, 512, CACHE_WAIT);
_mfence();
/* Re-enable Interrupts. */
_restore_interrupts(key);
for (loopIndex1 = 0; loopIndex1 < cCnt; loopIndex1++) {
for (loopIndex2 = 0; loopIndex2 < bCnt; loopIndex2++) {
for (loopIndex3 = 0; loopIndex3 < aCnt; loopIndex3++)
if (srcArrayPtr[loopIndex3] != dstArrayPtr[loopIndex3])
return FALSE;
srcArrayPtr = srcArrayPtr + srcBIdx;
dstArrayPtr = dstArrayPtr + dstBIdx;
}
if (abSync) {
srcFramePtr = srcFramePtr + srcCIdx;
srcArrayPtr = srcFramePtr;
dstFramePtr = dstFramePtr + dstCIdx;
dstArrayPtr = dstFramePtr;
}
else {
srcFramePtr = srcArrayPtr + srcCIdx - srcBIdx;
srcArrayPtr = srcFramePtr;
dstFramePtr = dstArrayPtr + dstCIdx - dstBIdx;
dstArrayPtr = dstFramePtr;
}
}
return TRUE;
}
static Int32 edma_ping_pong_xfer_gbl_region (Int32 instNum, Uint8 channelNum)
{
CSL_Edma3Handle hModule;
CSL_Edma3Obj edmaObj;
CSL_Edma3ParamHandle hParamPing;
CSL_Edma3ParamHandle hParamPong;
CSL_Edma3ChannelObj chObj;
CSL_Edma3CmdIntr regionIntr;
CSL_Edma3ChannelHandle hChannel;
CSL_Edma3ParamSetup myParamSetup;
CSL_Edma3Context context;
CSL_Edma3ChannelAttr chAttr;
CSL_Status status;
Uint32 loopIndex;
/* Start the EDMA PING-PONG test over the Global Region. */
printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d...\n", instNum, channelNum);
/* Initialize data */
for (loopIndex = 0; loopIndex < 256; loopIndex++)
{
srcBuff1[loopIndex] = loopIndex;
srcBuff2[loopIndex] = loopIndex;
dstBuff1[loopIndex] = 0;
dstBuff2[loopIndex] = 0;
}
print();
/* Module initialization */
if (CSL_edma3Init(&context) != CSL_SOK)
{
printf ("Error: EDMA module initialization failed\n");
return -1;
}
/* Open the EDMA Module using the provided instance number */
hModule = CSL_edma3Open(&edmaObj, instNum, NULL, &status);
if ( (hModule == NULL) || (status != CSL_SOK))
{
printf ("Error: EDMA module open failed\n");
return -1;
}
/* Channel open */
chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;
chAttr.chaNum = channelNum;
hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);
if ((hChannel == NULL) || (status != CSL_SOK))
{
printf ("Error: Unable to open EDMA Channel:%d\n", channelNum);
return -1;
}
if(!instNum)
{
/* For first EDMA instance there are only 2 TCs and 2 event queues
* Modify the channel default queue setup from 0 to 1
*/
if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_1) != CSL_SOK)
{
printf ("Error: EDMA channel setup queue failed\n");
return -1;
}
}
else
{
/* For EDMA instance 1 and 2 maximum of 4 TCs and 4 event queues are supported
* Change Channel Default queue setup from 0 to 3
*/
if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3) != CSL_SOK)
{
printf ("Error: EDMA channel setup queue failed\n");
return -1;
}
}
/* Map the DMA Channel to PARAM Block 2. */
CSL_edma3MapDMAChannelToParamBlock (hModule, channelNum, 2);
/* Obtain a handle to parameter set 2 */
hParamPing = CSL_edma3GetParamHandle(hChannel, 2, &status);
if (hParamPing == NULL)
{
printf ("Error: EDMA Get Parameter Entry failed for 2.\n");
return -1;
}
/* Obtain a handle to parameter set 1 */
hParamPong = CSL_edma3GetParamHandle(hChannel, 1, &status);
if (hParamPong == NULL)
{
printf ("Error: EDMA Get Parameter Entry failed for 1.\n");
return -1;
}
/* Setup the parameter entry parameters (Ping buffer) */
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN, \
0, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_DIS, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff1;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);
myParamSetup.dstAddr = (Uint32)dstBuff1;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);
myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
myParamSetup.cCnt = 1;
/* Ping setup */
if (CSL_edma3ParamSetup(hParamPing,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
/* Pong setup */
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN,\
1, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_EN, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff2;
myParamSetup.dstAddr = (Uint32)dstBuff2;
if (CSL_edma3ParamSetup(hParamPong,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
/* Interrupt enable (Bits 0-1) for the global region interrupts */
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x3;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
/* Trigger channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0;
regionIntr.intrh = 0;
/* Poll on IPR bit 0 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x1));
/* Clear the pending bit */
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);
/* Trigger Channel */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
/* Poll on IPR bit 2 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x2));
/* Check transfer by comparing the source and destination buffers */
if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff1, dstBuff1, TRUE) == FALSE)
{
printf ("Error: Verification (Source1/Destination1) Failed\n");
return -1;
}
if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff2, dstBuff2, TRUE) == FALSE)
{
printf ("Error: Verification (Source2/Destination2) Failed\n");
return -1;
}
/* Close channel */
if (CSL_edma3ChannelClose(hChannel) != CSL_SOK)
{
printf("Error: EDMA Channel Close failed\n");
return -1;
}
/* Close EDMA module */
if (CSL_edma3Close(hModule) != CSL_SOK)
{
printf("Error: EDMA Module Close failed\n");
return -1;
}
/* The test passed. */
return 0;
}
void main (void)
{
Uint8 channelNum;
Uint8 instNum = 0;
/* EDMA Instance 0: Supports only 16 DMA Channels. */
for (channelNum = 0; channelNum < 1; channelNum++)
{
if (edma_ping_pong_xfer_gbl_region(instNum, channelNum) < 0)
{
printf ("Error: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d FAILED\n", instNum, channelNum);
return;
}
printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d Passed\n", instNum, channelNum);
print();
}
return;
}
The output i am getting for the above is :
[C66xx_0] 252 252 0 0 /*Before initiation Transfer*/
[C66xx_0] 253 253 0 0
[C66xx_0] 254 254 0 0
[C66xx_0] 255 255 0 0
/* After transfer*/
[C66xx_0] Debug: Testing EDMA(0) Ping-Pong Test (Global) Region for Channel 0 Passed
[C66xx_0] 247 0 247 0
[C66xx_0] 84 0 84 0
[C66xx_0] 60 0 60 0
[C66xx_0] 5 0 5 0
The verify transfer function is fine and not giving any error. The values in srcBuff1 and srcBuff2 are getting changed.
Kindly let me know with my mistake.
Thanks
Varun