I am using DVR RDK 3.00,
in the ENC link, I know there is a parameter targetBitRate for setting the bitrate
but is there any min or max bitrate that the encoder can handle?
and is it the same in the case of decoder?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Minimum bitrate is 16384 bps.
Max bitrate depends on h264 profile and level selected.Pls see http://en.wikipedia.org/wiki/H264#Levels for details.