This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Wifi multi-role/wifi-direct functionality on dm814x board using com7 chip

Hi,

We were trying to bring up multi-role functionality on Jacinto4 board using com7(wl128) chipset.

 Link followed -

http://processors.wiki.ti.com/index.php/OMAP_Wireless_Connectivity_NLCP_Multi_Role_Configuration

 We had some queries with regard to the same -

1) Are 2 wlan interfaces required compulsorily for multirole functionality?

2) Does com7 chip have support for 2 wlan interfaces?

3) Is there dependency for support from base board for 2 wlan interfaces? Does Jacinto4(DM814x) board have support for 2 wlan interfaces?

I am facing issues in making both wlan intefaces work simultaneously on Jacinto4 using com7 chip. It returns as "device is busy" when trying to configure the 2 mode(station/softAP) on the second wlan interface created.

4) Is Jacinto4/com7 multirole/wifi-direct capable?

Please could you help us provide any pointers on these?

Regards,

Rohini