Hi
If we use 18 bit LCD display,then to which pins of AM3352 the RGB lines(each 6 bit) need to be connected in that 24bit Lcd controller ..
Regards
Rajan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
If we use 18 bit LCD display,then to which pins of AM3352 the RGB lines(each 6 bit) need to be connected in that 24bit Lcd controller ..
Regards
Rajan
Thanks Brandon
I have another query on this"How the grouping of each 8bit combination is done for RED GREEN and BLUE?"
Is it like
D0-D7 = Blue
D8-D15 = Green
D16-D24 = Red
or vice versa??
Regards
Is tha emissions you are saying is equal to EMI???
Usually we will have this kind of series resistor for High speed signal only so the LCD(3.5" &18 bit) I am going to use will operate with clock of 10MHz(Max),does this require series resistors along data and clock lines??
Regards