Other Parts Discussed in Thread: AM3352
Help. AM3352 was work for two weeks, powered on and booted successfully many times. Then one day, it stopped. The power light come on and stays on, and the screen backlist comes on, but that is all that happens. I gave it to my engineer mate, and he tested it.Below are the voltages at various places. As he says, at Y6 there was seen on oscilloscope 24MHz. And the DDRAM got so hot he stopped his tests.
I tried the SDK SD and the Android SD cards that came with the unit.
Can you advise what is wrong, and what we should do next?
His results are:
TP1 MON_REM2 (USB2412) 0V
TP2 GND
TP3 AM335X_USB0_CE 0V
TP4 USB0_ID 1.0V
TP5 VBAT (Backup) 4.8V
TP6 AM335X_USB1_CE 0V
TP7 PHY_PPS/GPIO (E'Net 0) 2.7V
TP8 PHY_PPS/GPIO (E'Net 1) 2.7V
TP9 PMIC_SLEEP 0.04V
TP10 CPU_Testout 0.7V
TP11 VBAT 4.8V
TP12 COM_BTUARTDEBUG 1.8V
TP13 GND
TP14 Codec_GPIO1 1.2V
TP15 COM_WL_RS232_RX 1.8V
TP16 Codec_GPIO2 1.2V
TP17 COM_WL_UART_DBG 1.8V
TP18 EMU3 0.1V
TP19 COM_WL_RS232_TX 1.8V
TP20 EMU2 0.1V
TP21 HD_SPKRM 1.2V
TP22 EMU4 0.1V
TP23 PGOOD (VTT) 3.3V
TP24 HS_SPKRM 1.2V
TP25 REFOUT (VTT) 0.75V
VDDSHV2 3.3V
VDDSHV3
VDDSHV4 3.3V
VDDSHV5
VDDSHV6 3.3V
VDDS_DDR 1.5V
VDD_CORE 1.2V
V3.3D 3.3V
None of these testpoints showed other than DC levels.
Y6 seen oscillating at 24MHz
U32 (DDRAM) running very hot, seriously uncomfortable on the skin. This caused me to discontinue the test.