Other Parts Discussed in Thread: DM385
Hi TI,
I'm using DM385 evm with latest EZSDK(ti-ezsdk_dm814x-evm_5_05_02_00).
I'm using the uart1 port for IR Receiver.I have followed the procedure, which has mentioned in the following user guide for configuring IR.
http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_CIR_Driver_User_Guide.
After that i came to know, this ezsdk kernel is not having the support for IR. Then i have downloaded the kernel from linux-omap3 git. which is having IR support.
http://arago-project.org/git/projects/?p=linux-omap3.git;a=summary.
Now my IR driver are properly registering and creating the device node(lirc0) with major and minor number.
I have tried the "mode2 -d /dev/lirc0" It will not show any o/p. I have probed the rx pin it is accepting the data, i can see that in CRO.
Also i tried the"ls /sys/class/rc/" Nothing is there in the rc folder.
I have done pin mux as follows for the rx pin.
static void ti813x_cir_pin_mux(void)
{
char mux_name[100];
sprintf(mux_name, "uart0_rin.uart1_rxd_mux0");
printk("cir pinmux\n");
omap_mux_init_signal(mux_name, OMAP_MUX_MODE0 |
TI814X_PULL_DIS | TI814X_INPUT_EN);
return;
}
What will be problem. Help me to resolve this issue...!!!!!!!!
Thanks & Regards
Ramappa