This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DM368 VPFE setup

Guru 15520 points

Hi,

I have a question about DM368 VPFE.

Capture data is 16bit YUV.
Parallel Input -> IPIPEIF -> ISIF -> SDRAM

If I want to  start sending the YUV data to DDR2 50 pixel clock after HD Sync,
do I need to setup both SPH register and FMTSPH register to 50 ?

By the way do I need to setup the following registers when the input data is YUV?
- FMTSPH
- FMTLNH
- FMTSLV
- FMTLNV
- FMTRLEN
- FMTHCNT

best regards,
g.f.