Other Parts Discussed in Thread: OMAP3503, TUSB1210
Hello,
I have a problem to configure an usbhost port of the omap3503
I have connected an USB3317 the the USBhost1 port of the omap3503. The pin CLKOUT (60MHz clock) of the USB3317 it is connected the the pin HSUSB1_CLK of the OMAP3503. Than I need to configure the HSUSB1 port in clock slave mode.
It is possible?
What are the register to configurre?