hello,
I use DM8168 for RDK3.5.
Where can set not display time limit for logo?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
I use DM8168 for RDK3.5.
Where can set not display time limit for logo?
thanks.
The questiuon is not clear. Do you want to increase boot logo display time?
Have you referred DVRRDK_03.50.00.05\dvr_rdk\docs\AppNotes\DM81xx_DVR_RDK_Boot_Logo_and_External_Device.pdf already?
hello,
I mean display the logo no time limit.
Maximum of 273 seconds to display a logo in the buffer size more than 1MB.
thanks.
Hi,
Do you want to display logo continuously? Don't you want to display any video or graphics data when you application actualy starts?
Regards,
Brijesh Jadav
Hi, Brijesh Jadav
Yes.
I want to control the display logo.
I test the display logo which the max is 273 sec 60 fps.
thanks.
Hi,
So do you wnat to display it for more than 273 seconds? Do you want to display any other video after your applicatin starts?
regards,
Brijesh
Hi TI friend,
I meet the same problem. Now, I can display logo at the uboot start. However, it is limited by the time, I want to display the logo always without the show time setting limited. How can I do?
Thanks!