This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does the AM335x DDR controller support "precharge all" command?

Guru 10570 points


Hello.

I would like to use DDR2 memory on AM335x.
There is a reg_t_rp(tRP) field in the SDRAM_TIM_1 register, which is used as precharge command.
But, there is not a field of tRPA which is used as precharge all command.

I think that the AM335x does not support precharge all command.
So, tRPA field is not needed. Is that right?

Best regards, RY