This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 ipnc3.5 about SALDRE function

Hi,all!

DM8127 run ipnc3.5 in the lowpower mode,we have a problem.

The ipnc3.5 support SALDRE when the camera output the resolution(such as 2560*1920) ,

but when I try to modify to the resolution(such as 2432 * 2048) using SALDRE, the camera cannot ouput images.

why?

  • 1- Have you tested 2432*2048 output without SLADRE? Does it work?

    2- what's the below print (during the boot time) when you run SLADRE with 2560*1920 and 2432*2048 respectively?

         Vps_printf("ROI dimensions of %d x %d are optimal for performance. Optimal dimension is %d x %d with processsing block= %d x %d. Num horz table= %d, vert table= %d, localBlockWidth= %d.\n",