This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358 fail to boot - crystal



Hi,

My processor fails to boot (have connected a UART cable to the debig port but I see no stream of 'C' characters).

The system clock 24MHz fails to output the desired frequency. Will this explain the issue with booting? Also, what will be the implication if the ground of the crustal I am using for the 24MHz clock connects to the general board ground? can this stop the processor booting?

Thanks.