Other Parts Discussed in Thread: AM3359
Hi,
I want to configure SPI1 in slave mode on the am3359. In the future I plan to use SPI0 for serial flash memory. This will require SPI0 in master mode.
So I will need SPI0 as master and SPI1 as slave but I'm not sure if this is possible?
The am335x Technical Reference Manual (http://www.ti.com/lit/ug/spruh73g/spruh73g.pdf) is a bit confusing...
- Section 24.1.1 says "Up to four SPI channels"
- Section 24.2 says "This device includes two instantiations of McSPI: SPI0 and SPI1."
- Section 24.33 says "McSPI is in slave mode when the bit MS of the register MCSPI_MODULCTRL is set."
- Section 24.4.1.7 shows only one McSPI Module Control Register (MCSPI_MODULCTRL)
Is it possible to have one master device and one slave device at the same time on the am3359?
Regards,
Fergal