This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIFA for 16bit device (C6747)

Other Parts Discussed in Thread: OMAP-L138

Hi,

Based on above red box, we are going to use EMA_BA[0] for EMA_A[13].
Also we build block as below.
We set the value as below and tested with above block.
1. CE2CFG = 0x843F91
2. EMIFA PINMUX Setting
Result is as followed
1. 16bit
We tested as 16bit, wave form of EMA_BA[1] is working, but EMA_BA[0] is not any feed back yet.
2. 8bit 
We also tested the system at 8bit, and EMA_BA[0] & EMA_BA[1] are working properly.
Could you tell me where we should check the system to work EMA_BA[0] at 16bit?
Thanks & Regards