Hi,
I have one question about AM3354 working condition.
Currently I’m investigating whether AM3354@1Ghz can run normally at ambient 85C.
Of course, I have no backdata for it, power consumption at max load or measured Tc.
Also 1Ghz is not yet released.
So I’d like to know if AM335x@800Mhz(extended grade, Tj 0 ~90) can operate normally up to what ambient temperature. How can I compute ambient range? I assume following conditions.
-AM335x 800Mhz
-Extended Grade
-load : LCD display+3D graphics+ 80% load of CPU + Ethernet
Thanks in advance.
BR,
Devin