hi
i am using the ICE board and SYS/BIOS 6_33_05_46 .and SDK is 1.0.0.07 I am implementing the example : am335x_sysbios_ind_sdk_1.0.0.7\sdk\examples\uartecho.
i have a qestion :
the ICE board use UART5. can you tell me how can display the output content? for example:UARTPutString(uartInstance,"Hello world..\n\r"); how can i contect with my PC using UART5.
This application needs that the serial port on the EVM connected to the host serial port via a NULL modem cable. A serial terminal application (like teraterm/hyperterminal/minicom) is running on the host. the sentence is writen in SDK.
can you telll if the EVM is the ICE board and the host is my PC?
thanks very much!
Best Regards.