This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GDB debugging from Qt creator doesn't work (AM335x Starter kit + the latest SDK kit)

Hi,

I have a problem with GDB debugging in Qt creator 2.7.0. I want to debug a simple Qt application (form with one label and one button) in my AM335x Starter kit (and the latest SDK kit). Debugger starts but reports two warnings:

Unable to find dynamic linker breakpoint function. > GDB will be unable to debug shared library initializers > and track explicitly loaded dynamic code.
> warning: Could not load shared library symbols for xx libraries, ... > Use the "info sharedlibrary" command to see the complete listing. > Do you need "set solib-search-path" or "set sysroot"?

Debugger doesn't work correctly - variables are not shown at all, if I add or remove breakpoint, debugger icon becomes grey.

Please, can somebody help me - what should I check (GDB init file?)?

Thanks, Edo

  • Hi Edo,

    Are you following a guide of some sort? Like this wiki for Sitara SDK?

    http://processors.wiki.ti.com/index.php/How_to_Run_GDB_on_CCSv5

    Thanks

    ki

  • Hi, Ki-Soo,

    I have found out:

    GDB debugging in QT Creator 2.4.1. works, in the latest version of QT Creator 2.7.0. GDB debugging doesn't work!.

    Is TI's SDK AM335xSDK 05_07_00_00 compatible with the latest version of QT Creator?

    What should I do - should I use old version of QT Creator (2.4.1.)?

    Below are two debugger logs (from old and the latest version of QT creator)


    - QT Creator 2.4.1. which works:

    Commands:

    86show version

    87-list-features

    88set print object on

    89set breakpoint pending on

    90set print elements 10000

    91set overload-resolution off

    92handle SIGSEGV nopass stop print

    93set unwindonsignal on

    94pwd

    95set width 0

    96set height 0

    97set auto-solib-add on

    98-interpreter-exec console "maintenance set internal-warning quit no"

    99-interpreter-exec console "maintenance set internal-error quit no"

    100-interpreter-exec console "disassemble 0 0"

    101-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/bridge.py')"

    102-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/dumper.py')"

    103-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/qttypes.py')"

    104-interpreter-exec console "bbsetup"

    105source /home/edo/ti-sdk-am335x-evm-05.07.00.00/.gdbinit

    106-interpreter-exec console "bbsetup"

    107set architecture arm-linux-generic-elf-32bit

    108set gnutarget arm-none-linux-gnueabi

    109-file-exec-and-symbols "/home/edo/terminal/terminal"

    110target remote 192.168.1.101:10002

    111-break-insert -f "\"terminal.cpp\":21"

    112maint print msymbols /tmp/gdb_ns_.Gx6766

    113-exec-continue

    114info shared

    115-stack-list-frames 0 20

    116-thread-info

    117-stack-select-frame 0

    118bb options:fancy,autoderef vars: expanded: typeformats: formats: watchers:

    <Rebuild Watchmodel 1>

    Response:

    sStarting debugger 'GdbEngine' for ABI 'arm-linux-generic-elf-32bit'...

    dStart parameters: 'terminal (on Remote Device)' mode: 6

    dABI: arm-linux-generic-elf-32bit

    dExecutable: /home/edo/terminal/terminal

    dDebugger: /home/edo/ti-sdk-am335x-evm-05.07.00.00/linux-devkit/bin/arm-arago-linux-gnueabi-gdb

    dProject: /home/edo/terminal (built: /home/edo/terminal)

    dQML server: 127.0.0.1:3768

    dRemote: 192.168.1.101:-1, arm-linux-generic-elf-32bit

    dGnu target: arm-none-linux-gnueabi

    dSysroot:

    dDebug Source Loaction:

    dSymbol file:

    dUsing server start script: Dumper libraries:

    d

    dDebugger settings:

    dUseAlternatingRowColours: false (default: false)

    dFontSizeFollowsEditor: false (default: false)

    dUseMessageBoxForSignals: true (default: true)

    dAutoQuit: false (default: false)

    dLogTimeStamps: false (default: false)

    dVerboseLog: false (default: false)

    dCloseBuffersOnExit: false (default: false)

    dSwitchModeOnExit: false (default: false)

    dUseDebuggingHelper: true (default: true)

    dUseCodeModel: true (default: true)

    dShowThreadNames: false (default: false)

    dUseToolTips: false (default: false)

    dUseToolTipsInLocalsView: false (default: false)

    dUseToolTipsInBreakpointsView: false (default: false)

    dUseAddressInBreakpointsView: false (default: false)

    dUseAddressInStackView: false (default: false)

    dLoadGdbInit: false (default: true) ***

    dScriptFile: /home/edo/ti-sdk-am335x-evm-05.07.00.00/.gdbinit (default: ) ***

    dWatchdogTimeout: 20 (default: 20)

    dAutoEnrichParameters: false (default: false)

    dTargetAsync: false (default: false)

    dMaximalStackDepth: 20 (default: 20)

    dAlwaysAdjustStackColumnWidths: false (default: false)

    dShowStandardNamespace: true (default: true)

    dShowQtNamespace: true (default: true)

    dSortStructMembers: true (default: true)

    dAutoDerefPointers: true (default: true)

    dAlwaysAdjustLocalsColumnWidths: false (default: false)

    dListSourceFiles: false (default: false)

    dSkipKnownFrames: false (default: false)

    dEnableReverseDebugging: false (default: false)

    dAllPluginBreakpoints: true (default: true)

    dSelectedPluginBreakpoints: false (default: false)

    dAdjustBreakpointLocations: true (default: true)

    dAlwaysAdjustBreakpointsColumnWidths: false (default: false)

    dNoPluginBreakpoints: false (default: false)

    dSelectedPluginBreakpointsPattern: .* (default: .*)

    dBreakOnThrow: false (default: false)

    dBreakOnCatch: false (default: false)

    dBreakOnWarning: false (default: false)

    dBreakOnFatal: false (default: false)

    dAlwaysAdjustRegistersColumnWidths: false (default: false)

    dAlwaysAdjustSnapshotsColumnWidths: false (default: false)

    dAlwaysAdjustThreadsColumnWidths: false (default: false)

    dAlwaysAdjustModulesColumnWidths: false (default: false)

    dState changed from DebuggerNotReady(0) to EngineSetupRequested(1).

    dQUEUE: SETUP ENGINE

    dCALL: SETUP ENGINE

    dTRYING TO START ADAPTER

    sNo server start script given.

    Preparing remote side ...

    Killing remote process(es)...

    Remote process started.

    Process /home/root/terminal created; pid = 2466

    Listening on port 10002

    dENABLING TEST CASE: 0

    dSTARTING /home/edo/ti-sdk-am335x-evm-05.07.00.00/linux-devkit/bin/arm-arago-linux-gnueabi-gdb -i mi -n

    dGDB STARTED, INITIALIZING IT

    <86show version

    <87-list-features

    <88set print object on

    <89set breakpoint pending on

    <90set print elements 10000

    <91set overload-resolution off

    <92handle SIGSEGV nopass stop print

    <93set unwindonsignal on

    <94pwd

    <95set width 0

    <96set height 0

    <97set auto-solib-add on

    <98-interpreter-exec console "maintenance set internal-warning quit no"

    <99-interpreter-exec console "maintenance set internal-error quit no"

    <100-interpreter-exec console "disassemble 0 0"

    <101-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/bridge.py')"

    <102-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/dumper.py')"

    <103-interpreter-exec console "python execfile('/usr/share/qtcreator/dumper/qttypes.py')"

    <104-interpreter-exec console "bbsetup"

    <105source /home/edo/ti-sdk-am335x-evm-05.07.00.00/.gdbinit

    <106-interpreter-exec console "bbsetup"

    dADAPTER SUCCESSFULLY STARTED

    dNOTE: ENGINE SETUP OK

    dState changed from EngineSetupRequested(1) to EngineSetupOk(3).

    dQUEUE: SETUP INFERIOR

    dState changed from EngineSetupOk(3) to InferiorSetupRequested(4).

    dQUEUE: SETUP INFERIOR

    dCALL: SETUP INFERIOR

    sSetting up inferior...

    <107set architecture arm-linux-generic-elf-32bit

    <108set gnutarget arm-none-linux-gnueabi

    <109-file-exec-and-symbols "/home/edo/terminal/terminal"

    >=thread-group-added,id="i1"

    >~"GNU gdb (GDB) 7.5\n"

    >~"Copyright (C) 2012 Free Software Foundation, Inc.\n"

    >~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is free software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitted by law. Type \"show copying\"\nand \"show warranty\" for details.\n"

    >~"This GDB was configured as \"--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi\".\nFor bug reporting instructions, please see:\n"

    >~"<http://www.gnu.org/software/gdb/bugs/>.\n"

    >&"show version\n"

    >~"GNU gdb (GDB) 7.5\n"

    >~"Copyright (C) 2012 Free Software Foundation, Inc.\n"

    >~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is free software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitted by law. Type \"show copying\"\nand \"show warranty\" for details.\n"

    >~"This GDB was configured as \"--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi\".\nFor bug reporting instructions, please see:\n"

    >~"<http://www.gnu.org/software/gdb/bugs/>.\n"

    >86^done

    dPARSING VERSION: 86^done

    d

    dSUPPORTED GDB VERSION GNU gdb (GDB) 7.5

    dCopyright (C) 2012 Free Software Foundation, Inc.

    dLicense GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

    dThis is free software: you are free to change and redistribute it.

    dThere is NO WARRANTY, to the extent permitted by law. Type "show copying"

    dand "show warranty" for details.

    dThis GDB was configured as "--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi".

    dFor bug reporting instructions, please see:

    d<http://www.gnu.org/software/gdb/bugs/>.

    dGNU gdb (GDB) 7.5

    dCopyright (C) 2012 Free Software Foundation, Inc.

    dLicense GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

    dThis is free software: you are free to change and redistribute it.

    dThere is NO WARRANTY, to the extent permitted by law. Type "show copying"

    dand "show warranty" for details.

    dThis GDB was configured as "--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi".

    dFor bug reporting instructions, please see:

    d<http://www.gnu.org/software/gdb/bugs/>.

    d

    dUSING GDB VERSION: 70500, BUILD: 2012

    >87^done,features=["frozen-varobjs","pending-breakpoints","thread-info","data-read-memory-bytes","breakpoint-notifications","ada-task-info","python"]

    dFEATURES: 87^done,data={features=["frozen-varobjs","pending-breakpoints","thread-info","data-read-memory-bytes","breakpoint-notifications","ada-task-info","python"]}

    d

    >&"set print object on\n"

    >88^done

    >&"set breakpoint pending on\n"

    >89^done

    >&"set print elements 10000\n"

    >90^done

    >&"set overload-resolution off\n"

    >91^done

    >&"handle SIGSEGV nopass stop print\n"

    >~"Signal Stop\tPrint\tPass to program\tDescription\n"

    >~"SIGSEGV Yes\tYes\tNo\t\tSegmentation fault\n"

    >92^done

    >&"set unwindonsignal on\n"

    >93^done

    >&"pwd\n"

    >~"Working directory /home/edo.\n"

    >94^done

    >&"set width 0\n"

    >95^done

    >&"set height 0\n"

    >96^done

    >&"set auto-solib-add on\n"

    >97^done

    >98^done

    >99^done

    >&"A syntax error in expression, near `0'.\n"

    >100^error,msg="A syntax error in expression, near `0'."

    >101^done

    >102^done

    >103^done

    >~"dumpers=[{type=\"QLinkedList\",formats=\"\"},{type=\"QSize\",formats=\"\"},{type=\"QFileInfo\",formats=\"\"},{type=\"QAbstractItemModel\",formats=\"\"},{type=\"std__stack\",formats=\"\"},{type=\"QTextDocument\",formats=\"\"},{type=\"QTJSC__JSValue\",formats=\"\"},{type=\"__gnu_cxx__hash_set\",formats=\"\"},{type=\"QStringList\",formats=\"\"},{type=\"QRegion\",formats=\"\"},{type=\"std__wstring\",formats=\"\"},{type=\"QString\",formats=\"Inline,Separate Window\",editable=\"true\"},{type=\"QTextCodec\",formats=\"\"},{type=\"QBasicAtomicInt\",formats=\"\"},{type=\"QScriptValue\",formats=\"\"},{type=\"QTime\",formats=\"\"},{type=\"QSharedData\",formats=\"\"},{type=\"std__vector\",formats=\"\",editable=\"true\"},{type=\"QRegExp\",formats=\"\"},{type=\"QTextCursor\",formats=\"\"},{type=\"QxXmlAttributes\",formats=\"\"},{type=\"QDateTime\",formats=\"\"},{type=\"QList\",formats=\"\"},{type=\"QStandardItem\",formats=\"\"},{type=\"std__deque\",formats=\"\"},{type=\"QFixed\",formats=\"\"},{type=\"QHash\",formats=\"\"},{type=\"QSharedPointer\",formats=\"\"},{type=\"QUrl\",formats=\"\"},{type=\"std__set\",formats=\"\"},{type=\"std__list\",formats=\"\"},{type=\"std__basic_string\",formats=\"\"},{type=\"QPoint\",formats=\"\"},{type=\"QHostAddress\",formats=\"\"},{type=\"QStack\",formats=\"\"},{type=\"QScopedPointer\",formats=\"\"},{type=\"QRectF\",formats=\"\"},{type=\"QMultiMap\",formats=\"\"},{type=\"QMapNode\",formats=\"\"},{type=\"QModelIndex\",formats=\"Normal,Enhanced\"},{type=\"QLocale\",formats=\"\"},{type=\"QSharedDataPointer\",formats=\"\"},{type=\"QVariant\",formats=\"\"},{type=\"string\",formats=\"\",editable=\"true\"},{type=\"QBasicAtomicPointer\",formats=\"\"},{type=\"QVector\",formats=\"\",editable=\"true\"},{type=\"QDate\",formats=\"\"},{type=\"QFile\",formats=\"\"},{type=\"QAtomicInt\",formats=\"\"},{type=\"TBuf\",formats=\"\"},{type=\"QWeakPointer\",formats=\"\"},{type=\"QSizeF\",formats=\"\"},{type=\"__m128\",formats=\"As Floats,As Doubles\"},{type=\"boost__optional\",formats=\"\"},{type=\"wstring\",formats=\"\"},{type=\"QPointF\",formats=\"\"},{type=\"TLitC\",formats=\"\"},{type=\"QRect\",formats=\"\"},{type=\"QByteArray\",formats=\"\"},{type=\"QMap\",formats=\"\"},{type=\"boost__shared_ptr\",formats=\"\"},{type=\"QChar\",formats=\"\"},{type=\"QDir\",formats=\"\"},{type=\"QPixmap\",formats=\"\"},{type=\"QFlags\",formats=\"\"},{type=\"std__map\",formats=\"\"},{type=\"QHashNode\",formats=\"\"},{type=\"QTemporaryFile\",formats=\"\"},{type=\"QObject\",formats=\"\"},{type=\"Eigen__Matrix\",formats=\"\"},{type=\"std__string\",formats=\"\",editable=\"true\"},{type=\"QImage\",formats=\"Normal,Displayed\"},{type=\"QSet\",formats=\"\"},],hasInferiorThreadList=\"1\"\n"

    >104^done

    >&"source /home/edo/ti-sdk-am335x-evm-05.07.00.00/.gdbinit\n"

    >105^done

    >~"dumpers=[{type=\"QLinkedList\",formats=\"\"},{type=\"QSize\",formats=\"\"},{type=\"QFileInfo\",formats=\"\"},{type=\"QAbstractItemModel\",formats=\"\"},{type=\"std__stack\",formats=\"\"},{type=\"QTextDocument\",formats=\"\"},{type=\"QTJSC__JSValue\",formats=\"\"},{type=\"__gnu_cxx__hash_set\",formats=\"\"},{type=\"QStringList\",formats=\"\"},{type=\"QRegion\",formats=\"\"},{type=\"std__wstring\",formats=\"\"},{type=\"QString\",formats=\"Inline,Separate Window\",editable=\"true\"},{type=\"QTextCodec\",formats=\"\"},{type=\"QBasicAtomicInt\",formats=\"\"},{type=\"QScriptValue\",formats=\"\"},{type=\"QTime\",formats=\"\"},{type=\"QSharedData\",formats=\"\"},{type=\"std__vector\",formats=\"\",editable=\"true\"},{type=\"QRegExp\",formats=\"\"},{type=\"QTextCursor\",formats=\"\"},{type=\"QxXmlAttributes\",formats=\"\"},{type=\"QDateTime\",formats=\"\"},{type=\"QList\",formats=\"\"},{type=\"QStandardItem\",formats=\"\"},{type=\"std__deque\",formats=\"\"},{type=\"QFixed\",formats=\"\"},{type=\"QHash\",formats=\"\"},{type=\"QSharedPointer\",formats=\"\"},{type=\"QUrl\",formats=\"\"},{type=\"std__set\",formats=\"\"},{type=\"std__list\",formats=\"\"},{type=\"std__basic_string\",formats=\"\"},{type=\"QPoint\",formats=\"\"},{type=\"QHostAddress\",formats=\"\"},{type=\"QStack\",formats=\"\"},{type=\"QScopedPointer\",formats=\"\"},{type=\"QRectF\",formats=\"\"},{type=\"QMultiMap\",formats=\"\"},{type=\"QMapNode\",formats=\"\"},{type=\"QModelIndex\",formats=\"Normal,Enhanced\"},{type=\"QLocale\",formats=\"\"},{type=\"QSharedDataPointer\",formats=\"\"},{type=\"QVariant\",formats=\"\"},{type=\"string\",formats=\"\",editable=\"true\"},{type=\"QBasicAtomicPointer\",formats=\"\"},{type=\"QVector\",formats=\"\",editable=\"true\"},{type=\"QDate\",formats=\"\"},{type=\"QFile\",formats=\"\"},{type=\"QAtomicInt\",formats=\"\"},{type=\"TBuf\",formats=\"\"},{type=\"QWeakPointer\",formats=\"\"},{type=\"QSizeF\",formats=\"\"},{type=\"__m128\",formats=\"As Floats,As Doubles\"},{type=\"boost__optional\",formats=\"\"},{type=\"wstring\",formats=\"\"},{type=\"QPointF\",formats=\"\"},{type=\"TLitC\",formats=\"\"},{type=\"QRect\",formats=\"\"},{type=\"QByteArray\",formats=\"\"},{type=\"QMap\",formats=\"\"},{type=\"boost__shared_ptr\",formats=\"\"},{type=\"QChar\",formats=\"\"},{type=\"QDir\",formats=\"\"},{type=\"QPixmap\",formats=\"\"},{type=\"QFlags\",formats=\"\"},{type=\"std__map\",formats=\"\"},{type=\"QHashNode\",formats=\"\"},{type=\"QTemporaryFile\",formats=\"\"},{type=\"QObject\",formats=\"\"},{type=\"Eigen__Matrix\",formats=\"\"},{type=\"std__string\",formats=\"\",editable=\"true\"},{type=\"QImage\",formats=\"Normal,Displayed\"},{type=\"QSet\",formats=\"\"},],hasInferiorThreadList=\"1\"\n"

    >106^done

    >&"set architecture arm-linux-generic-elf-32bit\n"

    >&"Undefined item: \"arm-linux-generic-elf-32bit\".\n"

    >107^error,msg="Undefined item: \"arm-linux-generic-elf-32bit\"."

    >&"set gnutarget arm-none-linux-gnueabi\n"

    >108^done

    >109^done

    <110target remote 192.168.1.101:10002

    >&"target remote 192.168.1.101:10002\n"

    >~"Remote debugging using 192.168.1.101:10002\n"

    Remote debugging from host 192.168.1.100

    >=thread-group-started,id="i1",pid="2466"

    sThread group i1 created

    dTaking notice of pid 2466

    >=thread-created,id="1",group-id="i1"

    sThread 1 created

    >=library-loaded,id="/lib/ld-linux.so.3",target-name="/lib/ld-linux.so.3",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/ld-linux.so.3 loaded

    >~"Reading symbols from /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3..."

    sReading /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3......

    >~"(no debugging symbols found)...done.\n"

    >~"Loaded symbols for /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3\n"

    >~"0x4bbc0790 in ?? () from /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3\n"

    >*stopped,frame={addr="0x4bbc0790",func="??",args=[],from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3"},thread-id="1",stopped-threads="all",core="0"

    >110^done

    dINFERIOR STARTED

    sAttached to stopped application

    sSetting breakpoints...

    dSetting breakpoints...

    <111-break-insert -f "\"terminal.cpp\":21"

    dATTEMPT SYNC

    >&"Cannot access memory at address 0x0\n"

    >111^done,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x0000a2b0",func="terminal::on_pushButton_clicked()",file="terminal.cpp",fullname="/home/edo/terminal/terminal.cpp",line="21",times="0",original-location="terminal.cpp:21"}

    dALL COMMANDS DONE; INVOKING CALLBACK

    <112maint print msymbols /tmp/gdb_ns_.Gx6766

    >&"maint print msymbols /tmp/gdb_ns_.Gx6766\n"

    >112^done

    dFOUND NON-NAMESPACED QT

    dNOTE: INFERIOR SETUP OK

    dState changed from InferiorSetupRequested(4) to InferiorSetupOk(6).

    dState changed from InferiorSetupOk(6) to EngineRunRequested(7).

    dQUEUE: RUN ENGINE

    dCALL: RUN ENGINE

    dNOTE: ENGINE RUN AND INFERIOR STOP OK

    dState changed from EngineRunRequested(7) to InferiorStopOk(14).

    dNOTE: INFERIOR RUN REQUESTED

    dState changed from InferiorStopOk(14) to InferiorRunRequested(10).

    sRunning requested...

    <113-exec-continue

    >113^running

    dNOTE: INFERIOR RUN OK

    dState changed from InferiorRunRequested(10) to InferiorRunOk(11).

    >*running,thread-id="all"

    >=library-loaded,id="/usr/lib/libQtGuiE.so.4",target-name="/usr/lib/libQtGuiE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtGuiE.so.4 loaded

    >=library-loaded,id="/usr/lib/libEGL.so",target-name="/usr/lib/libEGL.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libEGL.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libEGL.so loaded

    >=library-loaded,id="/usr/lib/libIMGegl.so",target-name="/usr/lib/libIMGegl.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libIMGegl.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libIMGegl.so loaded

    >=library-loaded,id="/usr/lib/libsrv_um.so",target-name="/usr/lib/libsrv_um.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libsrv_um.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libsrv_um.so loaded

    >=library-loaded,id="/usr/lib/libQtNetworkE.so.4",target-name="/usr/lib/libQtNetworkE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtNetworkE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtNetworkE.so.4 loaded

    >=library-loaded,id="/usr/lib/libQtCoreE.so.4",target-name="/usr/lib/libQtCoreE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtCoreE.so.4 loaded

    >=library-loaded,id="/lib/libpthread.so.0",target-name="/lib/libpthread.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libpthread.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libpthread.so.0 loaded

    >=library-loaded,id="/usr/lib/libstdc++.so.6",target-name="/usr/lib/libstdc++.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libstdc++.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libstdc++.so.6 loaded

    >=library-loaded,id="/lib/libm.so.6",target-name="/lib/libm.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libm.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libm.so.6 loaded

    >=library-loaded,id="/lib/libgcc_s.so.1",target-name="/lib/libgcc_s.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libgcc_s.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libgcc_s.so.1 loaded

    >=library-loaded,id="/lib/libc.so.6",target-name="/lib/libc.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libc.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libc.so.6 loaded

    >=library-loaded,id="/usr/lib/libgthread-2.0.so.0",target-name="/usr/lib/libgthread-2.0.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libgthread-2.0.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libgthread-2.0.so.0 loaded

    >=library-loaded,id="/lib/librt.so.1",target-name="/lib/librt.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/librt.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/librt.so.1 loaded

    >=library-loaded,id="/usr/lib/libglib-2.0.so.0",target-name="/usr/lib/libglib-2.0.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libglib-2.0.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libglib-2.0.so.0 loaded

    >=library-loaded,id="/usr/lib/libpng12.so.0",target-name="/usr/lib/libpng12.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libpng12.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libpng12.so.0 loaded

    >=library-loaded,id="/usr/lib/libz.so.1",target-name="/usr/lib/libz.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libz.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libz.so.1 loaded

    >=library-loaded,id="/usr/lib/libfreetype.so.6",target-name="/usr/lib/libfreetype.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libfreetype.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libfreetype.so.6 loaded

    >=library-loaded,id="/lib/libdl.so.2",target-name="/lib/libdl.so.2",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libdl.so.2",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libdl.so.2 loaded

    >=breakpoint-modified,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x0000a2b0",func="terminal::on_pushButton_clicked()",file="terminal.cpp",fullname="/home/edo/terminal/terminal.cpp",line="21",times="1",original-location="terminal.cpp:21"}

    >*stopped,reason="breakpoint-hit",disp="keep",bkptno="1",frame={addr="0x0000a2b0",func="terminal::on_pushButton_clicked",args=[{name="this",value="0xbe93ac08"}],file="terminal.cpp",fullname="/home/edo/terminal/terminal.cpp",line="21"},thread-id="1",stopped-threads="all",core="0"

    dNOTE: INFERIOR SPONTANEOUS STOP

    dState changed from InferiorRunOk(11) to InferiorStopOk(14).

    <114info shared

    sStopped at breakpoint 1 (1) in thread 1.

    <115-stack-list-frames 0 20

    <116-thread-info

    >&"info shared\n"

    >~"From To Syms Read Shared Object Library\n"

    >~"0x4bbc0790 0x4bbd842c Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3\n"

    >~"0x4c47a078 0x4ca692d0 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4\n"

    >~"0x40101fc0 0x40102118 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libEGL.so\n"

    >~"0x4003f93c 0x4004c0d0 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libIMGegl.so\n"

    >~"0x40051388 0x4006b5c4 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libsrv_um.so\n"

    >~"0x4cc9d144 0x4cd5b2b4 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtNetworkE.so.4\n"

    >~"0x4c06e0b0 0x4c1e9b58 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4\n"

    >~"0x4bd1bf20 0x4bd2a56c Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libpthread.so.0\n"

    >~"0x4be974a0 0x4bee0504 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libstdc++.so.6\n"

    >~"0x4bd531d8 0x4bd82100 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libm.so.6\n"

    >~"0x4be02658 0x4be08940 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libgcc_s.so.1\n"

    >~"0x4bbfd340 0x4bce5ab8 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libc.so.6\n"

    >~"0x4c0104d8 0x4c010644 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libgthread-2.0.so.0\n"

    >~"0x4bdc96a0 0x4bdccde8 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/librt.so.1\n"

    >~"0x4bf1c6a8 0x4bfb6a6c Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libglib-2.0.so.0\n"

    >~"0x4cc537d8 0x4cc6a9e0 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libpng12.so.0\n"

    >~"0x4bde17f8 0x4bdee734 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libz.so.1\n"

    >~"0x4cbd7910 0x4cc2a5a0 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libfreetype.so.6\n"

    >~"0x4bd408fc 0x4bd41624 Yes /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libdl.so.2\n"

    >114^done

    >115^done,stack=[frame={level="0",addr="0x0000a2b0",func="terminal::on_pushButton_clicked",file="terminal.cpp",fullname="/home/edo/terminal/terminal.cpp",line="21"},frame={level="1",addr="0x0000a9cc",func="terminal::qt_static_metacall",file="moc_terminal.cpp",fullname="/home/edo/terminal/moc_terminal.cpp",line="49"},frame={level="2",addr="0x0000ab24",func="terminal::qt_metacall",file="moc_terminal.cpp",fullname="/home/edo/terminal/moc_terminal.cpp",line="89"},frame={level="3",addr="0x4c18820c",func="QMetaObject::metacall(QObject*, QMetaObject::Call, int, void**)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4"},frame={level="4",addr="0x4c197858",func="QMetaObject::activate(QObject*, QMetaObject const*, int, void**)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4"},frame={level="5",addr="0x4ca5f0a4",func="QAbstractButton::clicked(bool)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"},frame={level="6",addr="0x4c7eafc0",func="??",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"},frame={level="7",addr="0x4c7eafc0",func="??",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"}]

    <117-stack-select-frame 0

    <118bb options:fancy,autoderef vars: expanded: typeformats: formats: watchers:

    >116^done,threads=[{id="1",target-id="Thread 2466",frame={level="0",addr="0x0000a2b0",func="terminal::on_pushButton_clicked",args=[{name="this",value="0xbe93ac08"}],file="terminal.cpp",fullname="/home/edo/terminal/terminal.cpp",line="21"},state="stopped",core="0"}],current-thread-id="1"

    >117^done

    >&"bb options:fancy,autoderef vars: expanded: typeformats: formats: watchers:\n"

    >~"data=[{iname=\"local.a\",name=\"a\",addr=\"0xbe93a344\",numchild=\"0\",type=\"int\",value=\"0\",},{iname=\"local.b\",name=\"b\",addr=\"0xbe93a340\",numchild=\"0\",type=\"int\",value=\"0\",},{iname=\"local.this\",name=\"this\",addr=\"0xbe93ac08\",addr=\"0xbe93ac08\",numchild=\"4\",origaddr=\"0xbe93ac08\",type=\"terminal\",value=\"{...}\",},,],typeinfo=[{name=\"aW50\",size=\"4\"},{name=\"dGVybWluYWw=\",size=\"24\"},]\n"

    >118^done

    <Rebuild Watchmodel 1>

    sFinished retrieving data

    - QT Creator 2.7.0. which doesn't work! - Data from variables is not shown:

    Commands:

    116show version

    117show debug-file-directory

    118set print object on

    119set breakpoint pending on

    120set print elements 10000

    121set overload-resolution off

    122handle SIGSEGV nopass stop print

    123set unwindonsignal on

    124set width 0

    125set height 0

    126-interpreter-exec console "set remotecache on"

    127-interpreter-exec console "maintenance set internal-warning quit no"

    128-interpreter-exec console "maintenance set internal-error quit no"

    129-interpreter-exec console "disassemble 0 0"

    130directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib

    131directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui

    132directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network

    133directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8

    134directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml

    135set sysroot /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS

    136set substitute-path /usr/src /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src

    137-interpreter-exec console "set auto-solib-add on"

    138-interpreter-exec console "python print 43"

    139-interpreter-exec console "pwd"

    140-interpreter-exec console "set target-async off"

    141-interpreter-exec console "set build-id-verbose 2"

    142-file-exec-and-symbols "/home/edo/test/test"

    143target remote tcp:192.168.1.101:10001

    144-break-insert -f "\"test.cpp\":21"

    145maint print msymbols /tmp/gdb_ns_.Df6914

    146-exec-continue

    147-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/bridge.py')"

    148-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/dumper.py')"

    149-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/qttypes.py')"

    150-interpreter-exec console "python qqStringCutOff = 10000"

    151-interpreter-exec console "bbsetup"

    152-thread-info

    153-stack-list-frames 0 20

    154-stack-select-frame 0

    155bb options:fancy,autoderef,dyntype vars: expanded:return,local,watch,inspect typeformats: formats: watchers:

    Response:

    sStarting debugger "GdbEngine" for ABI "arm-linux-generic-elf-32bit"...

    dStart parameters: 'test (on Remote Device)' mode: 6

    dABI: arm-linux-generic-elf-32bit

    dLanguages: c++

    dExecutable: /home/edo/test/test

    dDebugger: /home/edo/ti-sdk-am335x-evm-05.07.00.00/linux-devkit/bin/arm-arago-linux-gnueabi-gdb

    dProject: /home/edo/test (built: /home/edo/test)

    dQML server: 127.0.0.1:3768

    dRemote: 192.168.1.101:22

    dSysroot: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS

    dDebug Source Location: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml

    dSymbol file:

    dDumper libraries:

    dDebugger settings:

    dUseAlternatingRowColours: false (default: false)

    dFontSizeFollowsEditor: false (default: false)

    dUseMessageBoxForSignals: true (default: true)

    dAutoQuit: false (default: false)

    dLogTimeStamps: false (default: false)

    dVerboseLog: false (default: false)

    dCloseBuffersOnExit: false (default: false)

    dSwitchModeOnExit: false (default: false)

    dBreakpointsFullPath: false (default: false)

    dRaiseOnInterrupt: true (default: true)

    dUseDebuggingHelper: true (default: true)

    dUseCodeModel: true (default: true)

    dShowThreadNames: false (default: false)

    dUseToolTips: false (default: false)

    dUseToolTipsInLocalsView: false (default: false)

    dUseToolTipsInBreakpointsView: false (default: false)

    dUseAddressInBreakpointsView: false (default: false)

    dUseAddressInStackView: false (default: false)

    dLoadGdbInit: false (default: true) ***

    dAttemptQuickStart: false (default: false)

    dGdbStartupCommands: (default: )

    dGdbPostAttachCommands: (default: )

    dWatchdogTimeout: 20 (default: 20)

    dAutoEnrichParameters: false (default: true) ***

    dUseDynamicType: true (default: true)

    dTargetAsync: false (default: false)

    dWarnOnReleaseBuilds: true (default: true)

    dMultiInferior: false (default: false)

    dIntelFlavor: false (default: false)

    dMaximalStackDepth: 20 (default: 20)

    dAlwaysAdjustStackColumnWidths: false (default: false)

    dShowStandardNamespace: true (default: true)

    dShowQtNamespace: true (default: true)

    dSortStructMembers: true (default: true)

    dAutoDerefPointers: true (default: true)

    dAlwaysAdjustLocalsColumnWidths: false (default: false)

    dMaximalStringLength: 10000 (default: 10000)

    dListSourceFiles: false (default: false)

    dSkipKnownFrames: false (default: false)

    dEnableReverseDebugging: false (default: false)

    dAllPluginBreakpoints: true (default: true)

    dSelectedPluginBreakpoints: false (default: false)

    dAdjustBreakpointLocations: true (default: true)

    dAlwaysAdjustBreakpointsColumnWidths: false (default: false)

    dNoPluginBreakpoints: false (default: false)

    dSelectedPluginBreakpointsPattern: .* (default: .*)

    dBreakOnThrow: false (default: false)

    dBreakOnCatch: false (default: false)

    dBreakOnWarning: false (default: false)

    dBreakOnFatal: false (default: false)

    dBreakOnAbort: false (default: false)

    dAlwaysAdjustRegistersColumnWidths: false (default: false)

    dAlwaysAdjustSnapshotsColumnWidths: false (default: false)

    dAlwaysAdjustThreadsColumnWidths: false (default: false)

    dAlwaysAdjustModulesColumnWidths: false (default: false)

    dShowQmlObjectTree: true (default: true)

    dQmlInspector.ShowAppOnTop: false (default: false)

    dQmlInspector.FromQml: false (default: false)

    dState changed from DebuggerNotReady(0) to EngineSetupRequested(1) [master]

    dQUEUE: SETUP ENGINE

    dCALL: SETUP ENGINE

    dTRYING TO START ADAPTER

    dNOTE: REQUEST REMOTE SETUP

    sChecking available ports...

    Process /home/root/test created; pid = 2488

    Listening on port 10001

    dNOTE: REMOTE SETUP DONE: GDB SERVER PORT: 10001 QML PORT -1

    dENABLING TEST CASE: 0

    dSTARTING /home/edo/ti-sdk-am335x-evm-05.07.00.00/linux-devkit/bin/arm-arago-linux-gnueabi-gdb -i mi -n

    dGDB STARTED, INITIALIZING IT

    <116show version

    <117show debug-file-directory

    <118set print object on

    <119set breakpoint pending on

    <120set print elements 10000

    <121set overload-resolution off

    <122handle SIGSEGV nopass stop print

    <123set unwindonsignal on

    <124set width 0

    <125set height 0

    <126-interpreter-exec console "set remotecache on"

    <127-interpreter-exec console "maintenance set internal-warning quit no"

    <128-interpreter-exec console "maintenance set internal-error quit no"

    dTHE FOLLOWING COMMAND CHECKS AVAILABLE FEATURES. AN ERROR IS EXPECTED.

    <129-interpreter-exec console "disassemble 0 0"

    dEXAMINING /home/edo/test/test

    dELF SECTIONS: .interp .note.ABI-tag .hash .dynsym .dynstr .gnu.version .gnu.version_r .rel.dyn .rel.plt .init .plt .text .fini .rodata .ARM.extab .ARM.exidx .init_array .fini_array .jcr .dynamic .got .data .bss .ARM.attributes .comment .debug_aranges .debug_pubnames .debug_info .debug_abbrev .debug_line .debug_frame .debug_str .debug_loc .debug_macinfo .debug_pubtypes .debug_ranges .shstrtab .symtab .strtab

    sSetting up inferior...

    <130directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib

    <131directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui

    <132directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network

    <133directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8

    <134directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml

    <135set sysroot /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS

    <136set substitute-path /usr/src /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src

    <137-interpreter-exec console "set auto-solib-add on"

    <138-interpreter-exec console "python print 43"

    <139-interpreter-exec console "pwd"

    >=thread-group-added,id="i1"

    >~"GNU gdb (GDB) 7.5\n"

    >~"Copyright (C) 2012 Free Software Foundation, Inc.\n"

    >~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is free software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitted by law. Type \"show copying\"\nand \"show warranty\" for details.\n"

    >~"This GDB was configured as \"--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi\".\nFor bug reporting instructions, please see:\n"

    >~"<http://www.gnu.org/software/gdb/bugs/>.\n"

    >&"show version\n"

    >~"GNU gdb (GDB) 7.5\n"

    >~"Copyright (C) 2012 Free Software Foundation, Inc.\n"

    >~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is free software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitted by law. Type \"show copying\"\nand \"show warranty\" for details.\n"

    >~"This GDB was configured as \"--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi\".\nFor bug reporting instructions, please see:\n"

    >~"<http://www.gnu.org/software/gdb/bugs/>.\n"

    >116^done

    dPARSING VERSION: 116^done

    dSUPPORTED GDB VERSION GNU gdb (GDB) 7.5

    dCopyright (C) 2012 Free Software Foundation, Inc.

    dLicense GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

    dThis is free software: you are free to change and redistribute it.

    dThere is NO WARRANTY, to the extent permitted by law. Type "show copying"

    dand "show warranty" for details.

    dThis GDB was configured as "--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi".

    dFor bug reporting instructions, please see:

    d<http://www.gnu.org/software/gdb/bugs/>.

    dGNU gdb (GDB) 7.5

    dCopyright (C) 2012 Free Software Foundation, Inc.

    dLicense GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>

    dThis is free software: you are free to change and redistribute it.

    dThere is NO WARRANTY, to the extent permitted by law. Type "show copying"

    dand "show warranty" for details.

    dThis GDB was configured as "--host=i686-oesdk-linux --target=arm-oe-linux-gnueabi".

    dFor bug reporting instructions, please see:

    d<http://www.gnu.org/software/gdb/bugs/>.

    dUSING GDB VERSION: 70500, BUILD: 2012

    <140-interpreter-exec console "set target-async off"

    <141-interpreter-exec console "set build-id-verbose 2"

    >&"show debug-file-directory\n"

    >~"The directory where separate debug symbols are searched for is \"/usr/local/UsealongdefaultsdknametoinsurealongenoughtoolchainpathcanbeusedUseialongdefaultsdknametoinsurealongenoughtoolchainpathcanbeusedUseialong-2013.02/lib/armv7a-vfp-neon-oe-linux-gnueabi/debug\".\n"

    >117^done

    >&"set print object on\n"

    >118^done

    >&"set breakpoint pending on\n"

    >119^done

    >&"set print elements 10000\n"

    >120^done

    >&"set overload-resolution off\n"

    >121^done

    >&"handle SIGSEGV nopass stop print\n"

    >~"Signal Stop\tPrint\tPass to program\tDescription\n"

    >~"SIGSEGV Yes\tYes\tNo\t\tSegmentation fault\n"

    >122^done

    >&"set unwindonsignal on\n"

    >123^done

    >&"set width 0\n"

    >124^done

    >&"set height 0\n"

    >125^done

    >126^done

    >127^done

    >128^done

    >&"A syntax error in expression, near `0'.\n"

    >129^error,msg="A syntax error in expression, near `0'."

    >&"directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib\n"

    >&"Warning: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib: No such file or directory.\n"

    >~"Source directories searched: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:$cdir:$cwd\n"

    >130^done

    >&"directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui\n"

    >&"Warning: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui: No such file or directory.\n"

    >~"Source directories searched: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:$cdir:$cwd\n"

    >131^done

    >&"directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network\n"

    >&"Warning: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network: No such file or directory.\n"

    >~"Source directories searched: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:$cdir:$cwd\n"

    >132^done

    >&"directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8\n"

    >&"Warning: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8: No such file or directory.\n"

    >~"Source directories searched: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:$cdir:$cwd\n"

    >133^done

    >&"directory /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml\n"

    >&"Warning: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml: No such file or directory.\n"

    >~"Source directories searched: /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5declarative/src/qml:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/v8:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/network:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/gui:/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src/debug/qt5base/src/corelib:$cdir:$cwd\n"

    >134^done

    >&"set sysroot /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS\n"

    >135^done

    >&"set substitute-path /usr/src /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/src\n"

    >136^done

    >137^done

    >~"43\n"

    >138^done

    >~"Working directory /home/edo/qtcreator-2.7.0/bin.\n"

    >139^done

    dENGINE SUCCESSFULLY STARTED

    dNOTE: ENGINE SETUP OK

    dState changed from EngineSetupRequested(1) to EngineSetupOk(3) [master]

    dQUEUE: SETUP INFERIOR

    dState changed from EngineSetupOk(3) to InferiorSetupRequested(4) [master]

    dQUEUE: SETUP INFERIOR

    dCALL: SETUP INFERIOR

    <142-file-exec-and-symbols "/home/edo/test/test"

    >140^done

    >&"No symbol table is loaded. Use the \"file\" command.\n"

    >141^error,msg="No symbol table is loaded. Use the \"file\" command."

    >142^done

    <143target remote tcp:192.168.1.101:10001

    >&"target remote tcp:192.168.1.101:10001\n"

    >~"Remote debugging using tcp:192.168.1.101:10001\n"

    Remote debugging from host 192.168.1.100

    >=thread-group-started,id="i1",pid="2488"

    sThread group i1 created

    dTaking notice of pid 2488

    >=thread-created,id="1",group-id="i1"

    sThread 1 created

    >=library-loaded,id="/lib/ld-linux.so.3",target-name="/lib/ld-linux.so.3",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/ld-linux.so.3 loaded

    >~"Reading symbols from /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3..."

    sReading /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3......

    >~"(no debugging symbols found)...done.\n"

    >~"Loaded symbols for /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3\n"

    >~"0x4bbc0790 in ?? () from /home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3\n"

    >*stopped,frame={addr="0x4bbc0790",func="??",args=[],from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/ld-linux.so.3"},thread-id="1",stopped-threads="all",core="0"

    >143^done

    dINFERIOR STARTED

    sAttached to stopped application

    sSetting breakpoints...

    dSetting breakpoints...

    dATTEMPT BREAKPOINT SYNCHRONIZATION

    dTAKING OWNERSHIP OF BREAKPOINT 1 IN STATE 0

    <144-break-insert -f "\"test.cpp\":21"

    dBREAKPOINTS ARE NOT FULLY SYNCHRONIZED

    dATTEMPT SYNC

    dATTEMPT BREAKPOINT SYNCHRONIZATION

    dBREAKPOINTS ARE NOT FULLY SYNCHRONIZED

    >&"Cannot access memory at address 0x0\n"

    >144^done,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x0000a2c0",func="Test::on_pushButton_clicked()",file="test.cpp",fullname="/home/edo/test/test.cpp",line="21",times="0",original-location="test.cpp:21"}

    dATTEMPT BREAKPOINT SYNCHRONIZATION

    dBREAKPOINTS ARE SYNCHRONIZED

    dALL COMMANDS DONE; INVOKING CALLBACK

    <145maint print msymbols /tmp/gdb_ns_.Df6914

    >&"maint print msymbols /tmp/gdb_ns_.Df6914\n"

    >145^done

    dFOUND NON-NAMESPACED QT

    dNOTE: INFERIOR SETUP OK

    dState changed from InferiorSetupRequested(4) to InferiorSetupOk(6) [master]

    dState changed from InferiorSetupOk(6) to EngineRunRequested(7) [master]

    dQUEUE: RUN ENGINE

    dCALL: RUN ENGINE

    dNOTE: ENGINE RUN AND INFERIOR STOP OK

    sStopped.

    dState changed from EngineRunRequested(7) to InferiorStopOk(14) [master]

    dNOTE: INFERIOR RUN REQUESTED

    sRun requested...

    dState changed from InferiorStopOk(14) to InferiorRunRequested(10) [master]

    sRunning requested...

    <146-exec-continue

    >146^running

    dNOTE: INFERIOR RUN OK

    sRunning.

    dState changed from InferiorRunRequested(10) to InferiorRunOk(11) [master]

    >*running,thread-id="all"

    dNOTE: INFERIOR STILL RUNNING IN STATE InferiorRunOk.

    >=library-loaded,id="/usr/lib/libQtGuiE.so.4",target-name="/usr/lib/libQtGuiE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtGuiE.so.4 loaded

    >=library-loaded,id="/usr/lib/libEGL.so",target-name="/usr/lib/libEGL.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libEGL.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libEGL.so loaded

    >=library-loaded,id="/usr/lib/libIMGegl.so",target-name="/usr/lib/libIMGegl.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libIMGegl.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libIMGegl.so loaded

    >=library-loaded,id="/usr/lib/libsrv_um.so",target-name="/usr/lib/libsrv_um.so",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libsrv_um.so",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libsrv_um.so loaded

    >=library-loaded,id="/usr/lib/libQtNetworkE.so.4",target-name="/usr/lib/libQtNetworkE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtNetworkE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtNetworkE.so.4 loaded

    >=library-loaded,id="/usr/lib/libQtCoreE.so.4",target-name="/usr/lib/libQtCoreE.so.4",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libQtCoreE.so.4 loaded

    >=library-loaded,id="/lib/libpthread.so.0",target-name="/lib/libpthread.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libpthread.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libpthread.so.0 loaded

    >=library-loaded,id="/usr/lib/libstdc++.so.6",target-name="/usr/lib/libstdc++.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libstdc++.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libstdc++.so.6 loaded

    >=library-loaded,id="/lib/libm.so.6",target-name="/lib/libm.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libm.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libm.so.6 loaded

    >=library-loaded,id="/lib/libgcc_s.so.1",target-name="/lib/libgcc_s.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libgcc_s.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libgcc_s.so.1 loaded

    >=library-loaded,id="/lib/libc.so.6",target-name="/lib/libc.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libc.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libc.so.6 loaded

    >=library-loaded,id="/usr/lib/libgthread-2.0.so.0",target-name="/usr/lib/libgthread-2.0.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libgthread-2.0.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libgthread-2.0.so.0 loaded

    >=library-loaded,id="/lib/librt.so.1",target-name="/lib/librt.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/librt.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/librt.so.1 loaded

    >=library-loaded,id="/usr/lib/libglib-2.0.so.0",target-name="/usr/lib/libglib-2.0.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libglib-2.0.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libglib-2.0.so.0 loaded

    >=library-loaded,id="/usr/lib/libpng12.so.0",target-name="/usr/lib/libpng12.so.0",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libpng12.so.0",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libpng12.so.0 loaded

    >=library-loaded,id="/usr/lib/libz.so.1",target-name="/usr/lib/libz.so.1",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libz.so.1",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libz.so.1 loaded

    >=library-loaded,id="/usr/lib/libfreetype.so.6",target-name="/usr/lib/libfreetype.so.6",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libfreetype.so.6",symbols-loaded="0",thread-group="i1"

    sLibrary /usr/lib/libfreetype.so.6 loaded

    >=library-loaded,id="/lib/libdl.so.2",target-name="/lib/libdl.so.2",host-name="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/lib/libdl.so.2",symbols-loaded="0",thread-group="i1"

    sLibrary /lib/libdl.so.2 loaded

    >=breakpoint-modified,bkpt={number="1",type="breakpoint",disp="keep",enabled="y",addr="0x0000a2c0",func="Test::on_pushButton_clicked()",file="test.cpp",fullname="/home/edo/test/test.cpp",line="21",times="1",original-location="test.cpp:21"}

    >*stopped,reason="breakpoint-hit",disp="keep",bkptno="1",frame={addr="0x0000a2c0",func="Test::on_pushButton_clicked",args=[{name="this",value="0xbee53c18"}],file="test.cpp",fullname="/home/edo/test/test.cpp",line="21"},thread-id="1",stopped-threads="all",core="0"

    <147-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/bridge.py')"

    <148-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/dumper.py')"

    <149-interpreter-exec console "python execfile('/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/qttypes.py')"

    <150-interpreter-exec console "python qqStringCutOff = 10000"

    <151-interpreter-exec console "bbsetup"

    dNOTE: INFERIOR SPONTANEOUS STOP

    sStopped.

    dState changed from InferiorRunOk(11) to InferiorStopOk(14) [master]

    sStopped at breakpoint 1 (1) in thread 1.

    <152-thread-info

    >147^done

    >&"Traceback (most recent call last):\n"

    >&" File \"<string>\", line 1, in <module>\n"

    >&" File \"/home/edo/qtcreator-2.7.0/share/qtcreator/dumper/dumper.py\", line 6, in <module>\n"

    >&" import subprocess\n"

    >&"ImportError: No module named subprocess\n"

    >&"Error while executing Python code.\n"

    >148^error,msg="Error while executing Python code."

    >149^done

    >150^done

    >&"Undefined command: \"bbsetup\". Try \"help\".\n"

    >151^error,msg="Undefined command: \"bbsetup\". Try \"help\"."

    >152^done,threads=[{id="1",target-id="Thread 2488",frame={level="0",addr="0x0000a2c0",func="Test::on_pushButton_clicked",args=[{name="this",value="0xbee53c18"}],file="test.cpp",fullname="/home/edo/test/test.cpp",line="21"},state="stopped",core="0"}],current-thread-id="1"

    <153-stack-list-frames 0 20

    >153^done,stack=[frame={level="0",addr="0x0000a2c0",func="Test::on_pushButton_clicked",file="test.cpp",fullname="/home/edo/test/test.cpp",line="21"},frame={level="1",addr="0x0000a994",func="Test::qt_static_metacall",file="moc_test.cpp",fullname="/home/edo/test/moc_test.cpp",line="49"},frame={level="2",addr="0x0000aaec",func="Test::qt_metacall",file="moc_test.cpp",fullname="/home/edo/test/moc_test.cpp",line="89"},frame={level="3",addr="0x4c18820c",func="QMetaObject::metacall(QObject*, QMetaObject::Call, int, void**)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4"},frame={level="4",addr="0x4c197858",func="QMetaObject::activate(QObject*, QMetaObject const*, int, void**)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtCoreE.so.4"},frame={level="5",addr="0x4ca5f0a4",func="QAbstractButton::clicked(bool)",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"},frame={level="6",addr="0x4c7eafc0",func="??",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"},frame={level="7",addr="0x4c7eafc0",func="??",from="/home/edo/ti-sdk-am335x-evm-05.07.00.00/targetNFS/usr/lib/libQtGuiE.so.4"}]

    <154-stack-select-frame 0

    <155bb options:fancy,autoderef,dyntype vars: expanded:return,local,watch,inspect typeformats: formats: watchers:

    >154^done

    >&"bb options:fancy,autoderef,dyntype vars: expanded:return,local,watch,inspect typeformats: formats: watchers:\n"

    >&"Undefined command: \"bb\". Try \"help\".\n"

    >155^error,msg="Undefined command: \"bb\". Try \"help\"."

    dDUMPER FAILED: 155^error,data={msg="Undefined command: \"bb\". Try \"help\"."}


    Regards,

    Edo

  • Edvard Bregar said:

    GDB debugging in QT Creator 2.4.1. works, in the latest version of QT Creator 2.7.0. GDB debugging doesn't work!.

    Is TI's SDK AM335xSDK 05_07_00_00 compatible with the latest version of QT Creator?

    What should I do - should I use old version of QT Creator (2.4.1.)?

    I'm not sure myself. I'm going to move this to the Sitara fourms. They are most likely more aware of the various dependencies between the various versions of the software.

    Thanks

    ki