Is the "Deep power sleep" mode the most disabled state that the SGX can be in or can it be power gated to be completely shut off?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the "Deep power sleep" mode the most disabled state that the SGX can be in or can it be power gated to be completely shut off?
Hi Ryan,
I think the most disabled state that the SGX can be in is not just Deep power sleep (all clocks gated). It can be completely shut off through the PRCM register:
PM_SGX_PWRSTCTRL[1:0] POWERSTATE = 0x0 (OFF)
or you can execute the following command: root@dm816x-evm:~# /etc/init.d/pvr-init stop. After executing this command, SGX is powered-off, PM_SGX_PWRSTST[1:0] POWERSTATEST is equal to 0x0 (OFF state).
Best regards,
Pavel