Other Parts Discussed in Thread: TMS320C6678
Hi,
I'm working on two C6678 linked with an Hyperlink cable.
My attempts to generate an interrupt from core0 to core0 (local to remote) are successful.
Now I'm working in a multicore environment - let's say cores 0 & 1 are running on both remote and local DSPs. (core 0&1 <-- hyplnk --> core 0&1)
I'd like to be able to generate an interrupt from local core 0 to remote core 0 and remote core 1 independently.
1) Is it possible ?
The documentation says there are 64 events attached to Hyperlink (32 for the QMSS).
I've looked at the TMS320C6678 data manual p158 and I don't see how these events can be used to trigger interrupts.
2) Correct me if I'm wrong, but the System interrupt that will always be generated is VUSR_INT_0 (111) ?
3) How can the different events attached to Hyperlink be used to trigger different interrupts ?
Thanks.