Hi,
What is the lowest allowable frequency of a DDR2 which is connected to an L138 ?
For example, on page 30 oaf Micron MT47H64M16(product page)’s datasheet, the MAX clock cycle is listed as 8.0ns, which suggest lowest frequency is 125MHz.
However, in page 81 of the same document, it seems to have suggested that by disabling DLL, the DDR2 could even work “below” 25MHz.
On the L138 side, at many places in TRM SPRUH77 ch15 I read that the memory controller can disable DLL of DDR2, and register SDCR’s DDRDLL_DIS is used specifically for disabling DLL of DDR2.
Put these two together, should we understand it as: L138 can support MT47H64M16 running below 25MHz by setting SDCR'S DDRDLL_DIS→1? What is the lowest DDR2 frequency the L138 team has ever tested with?
Karl