This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts,
on our custom board with C6748 we have 16bit 512MB Micron nand flash on EMIFA. We have problem with speed of memory, reading is slower than we expected. In attached picture is detail of reading 512B (256 words) from flash. Yellow signal is flash memory chip select (EMA_CSn_3) and pink one is read enable (EMA_OEn) signal. We have external 24MHz crystal, core clock is set to 300Mhz and EMIFA clock is set to 150MHz in GEL file ( device_PLL0(0,24,1,0,1,1,5); ). Memory wait signal is not toggled during memory read.
In this post
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/55895.aspx
they have period of read signal shorter than 50ns with 100MHz EMIFA clock, while we have 600ns period with 150Mhz EMIFA clock.
Any suggestions why the read signal is so slow?
Thanks.
Jan
Hello RandyP,
I am not able to measure on pin B7 EMA_CLK, unfortunately this pin is not connected on PCB.
Today I am not able to debug with device and read directly EMIF timing register, but I tested LCDK nand example with following parameters
#define NAND_WRITE_SETUP_TIME_IN_NS (0u)
#define NAND_WRITE_STROBE_TIME_IN_NS (30u)
#define NAND_WRITE_HOLD_TIME_IN_NS (30u)
#define NAND_READ_SETUP_TIME_IN_NS (20u)
#define NAND_READ_STROBE_TIME_IN_NS (40u)
#define NAND_READ_HOLD_TIME_IN_NS (0u)
#define NAND_TURN_ARND_TIME_IN_NS (0u)
I tried also modify those parameters, but it has not much influence when the read period is 600ns and I chnage 20-30ns.
I will check and post exact EMIF timing registers values from debug in few days.
Regarding NAND device requirements it is able to handle read/write signal period down to 20ns according to datasheet.
Best Regards
Jan
Hello,
below is screenshot of EMIFA registers values, it looks like CE3CFG register uses reset values instead of values defined by macros.
Is any possibility to check EMIFA clock without measurement on EMIFA_CLK pin, like from some registers values?
Can anybody suggest how to propperly setup EMIFA and speed up nand flash memorry communication?
I am using nand_c674x_c6748_lcdkC6748 example project from starterware for testing.
Thanks.
Jan
Jan,
You do not need to check the EMA_CLK. With the values shown in CEnCFG, all of your timing parameters are set to their reset and maximum values, so that is why you timing is so slow.
The problem is not with the hardware but with the software not writing the values you want into those registers.
Please start from a working example, look through your software, and you can try to find what has changed from that example to your own software.
Regards,
RandyP
Hello RandyP,
finnaly I found the problem in driver emifa.c in starterware, this thread in starterware forum helped me find solution
http://e2e.ti.com/support/embedded/starterware/f/790/t/187844.aspx
Now I am able to tune memory clocking.
Thank You for support!
Jan