Hi all,
I am using DVRRDK 3.0 with DM8168EVM. I added an objection detection algorithm in DSP side of McFW. The codes can be built successfully.
However when I run the codes, the codes could only run the First frame,the second frame,it run dead。
I have track the code step by step in CCSv5,when it run dead,the Console output is as following:
[C674X_0] A0=0x0 A1=0x0
[C674X_0] A2=0x0 A3=0x1
[C674X_0] A4=0xb0254e80 A5=0x0
[C674X_0] A6=0x162 A7=0x0
[C674X_0] A8=0x9f191f24 A9=0x0
[C674X_0] A10=0xb463d0b0 A11=0xb4000000
[C674X_0] A12=0xb447a180 A13=0x9ffbfe18
[C674X_0] A14=0x0 A15=0x7843
[C674X_0] A16=0xb0001004 A17=0x0
[C674X_0] A18=0xfffe763a A19=0xffffffff
[C674X_0] A20=0xff A21=0xb4012abe
[C674X_0] A22=0x4000 A23=0xb463d101
[C674X_0] A24=0xfffe8000 A25=0xb463d100
[C674X_0] A26=0x9 A27=0x9
[C674X_0] A28=0x0 A29=0xc000
[C674X_0] A30=0xb0254ea0 A31=0xb0254e48
[C674X_0] B0=0x1d020100 B1=0x66a0010
[C674X_0] B2=0x0 B3=0x1
[C674X_0] B4=0x1d060300 B5=0x9ffb81fc
[C674X_0] B6=0x66a0010 B7=0x9ffb818c
[C674X_0] B8=0x13e B9=0x1
[C674X_0] B10=0xb4012c00 B11=0x9ffbfe18
[C674X_0] B12=0xb463ca18 B13=0x0
[C674X_0] B14=0x9ffbfc4c B15=0x9f251020
[C674X_0] B16=0x8a010e B17=0x0
[C674X_0] B18=0x1 B19=0xff
[C674X_0] B20=0x0 B21=0x12abe
[C674X_0] B22=0x13f B23=0xee
[C674X_0] B24=0x1 B25=0x0
[C674X_0] B26=0x1 B27=0xffffff80
[C674X_0] B28=0xffffff80 B29=0x13f
[C674X_0] B30=0x0 B31=0x9f251020
[C674X_0] NTSR=0x1020f
[C674X_0] ITSR=0x20d
[C674X_0] IRP=0x9f1891d4
[C674X_0] SSR=0x0
[C674X_0] AMR=0x0
[C674X_0] RILC=0x0
[C674X_0] ILC=0x0
[C674X_0] Exception at 0x0
[C674X_0] EFR=0x2 NRP=0x0
[C674X_0] Internal exception: IERR=0x1
[C674X_0] Instruction fetch exception
[C674X_0] ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x9f1891d4, sp = 0x9f251020.
[C674X_0] To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
[C674X_0] xdc.runtime.Error.raise: terminating execution
I do not know what reason ? Could you give me some suggestion?It is a Memory problems??or something else?
Thanks.
JQ Zhao