Hi all,
I am using DVRRDK 3.0 with DM8168EVM. I am developing my application in McFW.Now I want to add some new section to place my data 、heap. So I should modified the BIOS_c6xdsp.cfg. I added :
Program.sectMap[".MyMem"] = "DDR3_DSP";
Program.sectMap[".MyHeap"] = "DDR3_DSP";
But the remaining space of DDR3_DSP is too small for my data and heap.
So I modified it to SR1,when I build it,some errors:
"/usr/local/DVRRDK_03_00_00_00/DVRRDK_03.00.00.00/dvr_rdk/../dvr_rdk/bu
ild/dvr_rdk/obj/ti816x-
evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 260: error:
run placement fails for object ".MyHeap", size 0x4000007 (page 0).
Available ranges:
SR1 size: 0xd000000 unused: 0x0 max hole: 0x0
So, what can I use instead of DDR3_DSP?? or other suggestions you have??
Thanks.
JQ Zhao