This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with using the Arago git repository

Follow the instructions on U-Boot Build. in teh MCSDK UG Chapter Exploring page 5

 

try to do the instruction git clone

 

Got error message "Unable to connect to arago-project.org"

I assume I need to set the proxi

1. Does any one have an working TI example for wgetrc?   The reference is into generic Linux example and I have no idea what is needed and what is not

2. Does anyone have an example of the export statements that I have to add to .bashrc file? 

Thanks

 

Ran