Hi all, I recently found that I have a development kit TMS320C6000 but I think it is a very old development platform, I would like to know if I want to use it, which CCS should I use? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all, I recently found that I have a development kit TMS320C6000 but I think it is a very old development platform, I would like to know if I want to use it, which CCS should I use? Thanks.
The best way to develop on most TI DSP based development platforms is in the Code Composer studio environment. There latest version of Code composer studio is version 5.x but since you are using an old platform, you might need to check what version of CCS on which the software stack for the platform is built. Most software can be easily ported from earlier versions of CCSv 3.3/ CCSv4 to CCSv5
Regards,
Rahul
hı
ı am usıng TMS320c6711 board wıth CCS v5.5 but ıt ıs gıvıng me the problem
Error connecting to the target:
Error 0x80000200/-148
Fatal Error during: OCS,
Error generated by SD scan controller module
Is this driver issue?
I have connected the DSK C6711 through the printer port to the pc.
Plz help
Thanks in advance
Hi Fiaz,
I would like to post your CCS related queries in CCS forum.
http://e2e.ti.com/support/development_tools/code_composer_studio/default.aspx