Other Parts Discussed in Thread: 4430
- When TRUNCATIONENABLE bit in DISPC_WB_ATTRIBUTES is set and I'm enabling writeback, I have SYNC_LOST interrupt
- When TRUNCATIONENABLE bit in DISPC_WB_ATTRIBUTES is reset and I'm enabling writeback, I have instant kernel crash, unfortunately without any message on serial console.
When I was comparing register settings with working driver for kernel ti-ubuntu-2.6.35-991.5, truncation was disabled for ARGB32 format. I compared register settings of DISPC between two kernels (3.4 and 2.6) and I haven't noticed any significant differences.