This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x cache coherence procedures

Hi,

From a document for the TMS320C674x describing the cache and how it works (Cache User's Guide) I got the information that buffers need to be aligned and n times the size of a cache line.
Now StarterWare includes functions like "CacheDataInvalidateBuff()" and "CacheDataCleanBuff()" to get the memory and cache coherent. Both functions allow to tell how many bytes to be invalidated/cleaned.
Question: Should this number of bytes be n times the size of the cache line or does the functions correct the value to n times the size of the cache line?

Example: Is this correct (?):

CacheDataInvalidateBuff(&buffer[0], 3);

or should it be:

CacheDataInvalidateBuff(&buffer[0], 64);

Thanks.

Best regards,
Patrick




  • Patrick,

               The right way is to mention the size (number of bytes), which is multiple of cache line size. And ensure the starting address is aligned.

               If not the API will align (floor) to the lower address which is multiple of cache line size. But this might lead to confusions.

    Regards

    Baskaran