Hi,
I am working in aplication that need to use linux on master
and communicate with others cores that use SYS/BIOS.
I am using TMDSEVM6678LE and I am debugging using
the mezzanine xds560v2 that comes with the board.
I was following this guide Linux-c6x-2.0-GA User Guide
but when I try the step Executing the DSS script it seems
that there is no emulator connect. I am using linux ubuntu
12.04 LTS running on virtual box. I get the blackhawk xds560 appears in the list
of devices connected in the virtual machine but when I run Executing the DSS script
it does not detect the mezzanine xds560v2.
The questions are:
1) Is this Linux-c6x-2.0-GA User Guide what I need to work with a linux on master and SYS/BIOS on slaves cores from emulation using mezzanine xds560v2?
if not tell what guide or document or demo I can follow to get the what I want.
2) Is there any way to follow Linux-c6x-2.0-GA User Guide from windows?
If not Could you please help to get connexion of xds 560v2 to follow Linux-c6x-2.0-GA User Guide?