This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about the use problem of the remained pin for the MMC/SD on the OMAPL13X

Hi:

     I have met a problem about using the MMC/SD1 on the OMAPL13x: I have used the four data pins(data0-data3), while other 4 data pins(data4-data7) will not be used. But I want to use the remained data pins(data4-data7) ,these pins will be used as the GPIO port function in my product. Can I do it? Will this application affect the MMC/SD function?

      If I use MMC/SD function,the used data pins of MMC/SD interface can't be used as GPIO. Is it so?

      Thanks!