This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670 TCP3D problem



I use DSP 6670 with Windows 7 PC  in my work. I need to use a turbo decoder for an LTE application, so I try to run tcp3d example from C:\ti\pdk_C6670_1_0_0_20\packages\ti\drv\exampleProjects\tcp3dExampleProject,
but the result is not as I expected .
I want to run TCP3D_A with core0 and TCP3D_B with core1  parallelly,
and I have modified  the codes as follows:
static Int32 enable_tcp3d (void)
{ int CSL_PSC_PD_TCP3D;
  int  CSL_PSC_LPSC_TCP3D;
#ifdef SIMULATOR_SUPPORT
    /* TCP3D power domain is turned OFF by default.
     * It needs to be turned on before doing any TCP3D device register access.
     * This is not required for the simulator. */
 dspCoreID           = CSL_chipReadDNUM();
 if(dspCoreID==0)
 {   CSL_PSC_PD_TCP3D=CSL_PSC_PD_TCP3D_A;
 CSL_PSC_LPSC_TCP3D=CSL_PSC_LPSC_TCP3D_A;
 }
else
{  CSL_PSC_PD_TCP3D=CSL_PSC_PD_TCP3D_B ;
 CSL_PSC_LPSC_TCP3D=CSL_PSC_LPSC_TCP3D_B;
}
    /* Set TCP3D Power domain to ON */        
    CSL_PSC_enablePowerDomain (CSL_PSC_PD_TCP3D);
    /* Enable the clocks too for TCP3D */
    CSL_PSC_setModuleNextState (CSL_PSC_LPSC_TCP3D, PSC_MODSTATE_ENABLE);
    /* Start the state transition */
    CSL_PSC_startStateTransition (CSL_PSC_PD_TCP3D);
    /* Wait until the state transition process is completed. */
    while (!CSL_PSC_isStateTransitionDone (CSL_PSC_PD_TCP3D));
    /* Return TCP3D PSC status */
    if ((CSL_PSC_getPowerDomainState(CSL_PSC_PD_TCP3D) == PSC_PDSTATE_ON) &&
        (CSL_PSC_getModuleState (CSL_PSC_LPSC_TCP3D) == PSC_MODSTATE_ENABLE))
    {
        /* TCP3D ON. Ready for use */            
        return 0;
    }
    else
    {
        /* SRIO Power on failed. Return error */            
        return -1;            
    }
#else
    /* PSC is not supported on simulator. Return success always */
    return 0;
#endif
}
then I load the program both on core0 and core1 and start them at the same time.
It turns to have problems.How can I fix it?