This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No access to USB register (USBSS, USB0, ...)

Hello,

we are using the TI AM335x Starterkit and modified it for debugging with JTAG.

Download und debugging with IAR Workbench via I-Jet is possible.

After downloading, our application works.  But  we don't have access to the registers in the range from 0x4740000 to 0x47FFFFFF.

For example a read access to USBSS.REVREG leads to an exception. In this address range the memory window of the IAR Workbench shows dashes only.

The register at CM_PER and PRM_PER are set to the values:

 PM_PER_RSTCTRL = 0x00000003
 PM_PER_PWRSTST = 0x1E60007
 PM_PER_PWRSTCTRL = 0xEE0000EB

 CM_PER_L3S_CLKSTCTRL = 0x000A
 CM_PER_L3_CLKSTCTRL = 0x001E

Is there a register, I forgot to initialize?

What must I do, to have access to the USB register (USBSS, USB0, ...)?

King regards,

Stefan