Other Parts Discussed in Thread: DM3730
Hello,everyone:
I'm using BB-XM rev c(DM3730), now i bought a LCD the timing is below:
Item Symbol Min. Typ. Max. Unit
Frequency 1/Tc -- 100 -- MHz
Vertical Total Time TV -- 800 -- TH
Vertical Active Display Period TVD -- 768 -- TH
Vertical Blanking Period TVB -- 32 -- TH
Horizontal Total Time TH -- 2084 -- Tc
Horizontal Active Display Period THD -- 1024 -- Tc
Horizontal Blanking Period THB TH -- 1060 -- Tc
i see it a DE mode,but i find BB-XM use SYNC mode. I want to know, how can i to configure the LCD timings? thanks.
BR