This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can i to configure the LCD timings

Hello,everyone:

I'm using BB-XM rev c(DM3730) runs android2.3.4 with rowboat-dsp, now i bought a LCD the timing is below:

Item                                            Symbol     Min.   Typ.     Max.    Unit 

Frequency                                   1/Tc         --      100      --        MHz 
Vertical Total Time                       TV           --       800   --         TH 
Vertical Active Display Period      TVD        --      768      --        TH 
Vertical Blanking Period               TVB        --       32       --        TH 
Horizontal Total Time                   TH          --       2084   --        Tc 
Horizontal Active Display Period  THD       --      1024    --        Tc 
Horizontal Blanking Period           THB TH  --     1060     --        Tc

it's a DE mode,but i find BB-XM use SYNC mode. I want to know, how can i to configure the LCD timings? thanks.

BR