This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM365 Embedded Development need Linux?



Hello All

I am new with this IC and would like to ask if development with the TMS320DM365 DMSoc requires Linux if it will be used for an embedded

application such as video recording. I understand Linux is only for cases the platform need to interact with the PC for HD media. Is that correct?

My application is totally autonomous, would be right to use CCS only?

Thank you very much.

  • Hi,

    Reuven Levin said:
    I understand Linux is only for cases the platform need to interact with the PC for HD media. Is that correct?

    If your system is complex and want use Linux OS services to develop your system, then you can go for it.

    Reuven Levin said:
    My application is totally autonomous, would be right to use CCS only?

    Yes you can got CCS. you can develop your produce using CCS and TI BIOS etc..

    Thanks,

    Veeranna