This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootloader hangsforever in OMAP EVM MAIN BOARD

Hi

I am using omap 3530(OMAP EVM MAIN BOARD) with  x-loader 1.42,  after x-loader up comes it stops the booting  at  "Starting OS Bootloader..." and hangs forever. How to overcome from this problem?.

/*******************************************/

Texas Instruments X-Loader 1.42
Starting OS Bootloader...

/*******************************************/

  • Hi Srinivas,

    The message "Starting OS Bootloader..." shows that the x-loader (MLO) completes its work and then go to run the u-boot but the the u-boot never runs. There are some possible reasons for this stuck of system:

    • The u-boot is incorrect or not presents
    • If you expect to boot from the sd card which is prepared correctly but the system boots from nand and there is only x-loader.

    I suggest you to change the x-loader with other one with different version and you should see on the console the version of the new x-loader to ensure that the system booting from the right place. You can use the prebuilt files of DVSDK 4.03 which could download from the link:

    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_4_00/latest/index_FDS.html

    The version on the x-loader will be 1.51.

    BR

    Tsvetolin Shulev