Can someone provide a high level understanding of how a compiled software application gets from the computer running CCS to SPI NOR Flash attached to the SPI pins of the C6657?
Assuming XDS560v2 is connected from PC to target board via 60 pin connection (MIPI).
Assuming the processor is up running another application, does it halt when the emulator talks to the DSP (via JTAG) to tell it that it is going to be programmed to load the SPI?
Thank you,
Thomas