Hallo,
We are developing our custom board based on AM3359 and starter kit schematics. Due to the errata + current consumption restrictions of the internal RTC in AM335x, we would like to disable it and use the RTC in the power management IC.
After reading the forums and the schematic checklist wiki, I am a little confused about the proper pin configuration for this particular mode. Especially regarding PWRONRSTn and External LDO for VDDS_RTC.
I have listed the configuration as per my understanding and would be very thankful if someone could confirm the following pin configuration for the RTC disabled mode.
Pin | RTC feature disabled Configuration |
VDDS_RTC | external LDO |
CAP_VDD_RTC | VDD_CORE |
RTC_KALDO_ENn | VDDS_RTC |
RTC_PWRONRSTn | VSS |
PMIC_POWER_EN | No Connect |
EXT_WAKEUP | VSS |
XTAL Pins | No Connect |
Thanks a lot in advance.
Ram