This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ftp Server - EVM 8148

Dear all,

I would like to know how can I transfer file via ftp server. how can I install ftp server in the EVM.

In addition, how can I do remote debug by QT.

please answer me step by step, it's the first time I work with Linux and EVM 8148.

Regard,

Yoel

  • thanks,

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.04.22 15:26:15 =~=~=~=~=~=~=~=~=~=~=~=
    ge U-Boot will now be auto-loaded
    Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
    Hit any key to stop autoboot:  0 
    reading u-boot.bin
    
    210400 bytes read
    ## Starting application at 0x80800000 ...
    
    
    U-Boot 2010.06 (Dec 26 2012 - 18:12:01)
    
    TI8148-GP rev 2.1
    
    ARM clk: 600MHz
    DDR clk: 400MHz
    
    I2C:   ready
    DRAM:  2 GiB
    NAND:  HW ECC BCH8 Selected
    No NAND device found!!!
    0 MiB
    MMC:   OMAP SD/MMC: 0
    *** Warning - bad CRC or NAND, using default env                          .:;rrr;;.                   
                        ,5#@@@@#####@@@@@@#2,             
                     ,A@@@hi;;;r5;;;;r;rrSG@@@A,          
                   r@@#i;:;s222hG;rrsrrrrrr;ri#@@r        
                 :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:      
                B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B     
               @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@    
              @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@   
             @@;;rrsrrs@MB#@@@@@###@    @#;rsrsrsrsrr;r2ir @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
           @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
           @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
           M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
           :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
            @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@ 
             @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@  
             ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;  
              r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r   
               ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H      
             
                    .A@@         ;&@@@@MhXS5i5S                       :ihM#@@@@@##hs,                
    
    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:40:5f:c2:3e:7:93
    cpsw
    Hit any key to stop autoboot:  3  1 reading boot.scr
    
    354 bytes read
    Running bootscript from MMC/SD to set the ENV...
    
    151674 bytes read
    reading uImage
    age Name:   Arago/2.6.37-Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2796380 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... arting kernel ...
    
     Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Wed Dec 26 18:11:35 IST 2012
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing : 0xf000
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 160648
    Kernel command line: console=ttyO0,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M  notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 364MB 270MB = 634MB total
    Memory: 637324k/637324k available,  - 0xf8000000   ( 528 MB)
        lowmem  : 0xc0000000 - 0xd6c00000   ( 364 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .init : 0xc0008000 - 0xc003d000   ( 212 kB)
          .tex49000   (5168 kB)
          .data : 0xc054a000 - 0xc05970c0   ( 309 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC apts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ400
    Trying to install interrupt handler for IRQ401
    Trying to install interrupt handler for IRQ402
    Trying to install interrupt handler for IRQ403
    404
    Trying to install interrupt handler for IRQ405
    Trying to install interrupt 
    Trying to install type control for IRQ407
    Trying to set irq flags for IRQ407
    0000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buge driver init not yet happened.Faulting!
    omap_voltage_add_dev: VDD specified does not exist!
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core,request GPMC CS
    Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
    registered ti81xx_vpss device
    registered ti81xx_vidout device
    registered ti81xx on-chip HDMI device
    registered ti81xx_fb device
    registered ti81xx_vin device
    ti81xx_pcie: Invoking PCI BIOS...
    ti81xx_pcie: Setting up Host Controller...
    ti81xx_pcie: Register base mapped @0xd7020000
    ti81xx_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers enabled
    bio: create slab <bio-0> atSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    USBSS revision 4ea2080b
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    pcf857x 1-0021: gpios 128..143 on a pcf8575
    regulator: VRTC: 1800 mV 
    regulator: VIO: 1500 mV 
    regulator: VDD1: 600 <--> 1500 mV at 1200 mV 
    regulator: VDD2: 600 <--> 1500 mV at 1200 mV 
    regulator: VDDCT3300 mV at 1800 mV 
    regulator: LDO3: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO4: 11: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO6: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO7: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO8: 1100 <--> 3300 mV at 1800 mV 
    tps65910 1-002d: No interrupt support, no core IRQ
    omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, host, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    MUSB controller-0 revision 4ea20800
    musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: SB HDRC host driver
    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb1: SerialNumber: musb-hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port db-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18
    musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    MUSB controller-1 revision 4ea20800
    musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: l family 2
    IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
    TCP established hash table entries: 65536 (order: 7, 524288 bytes)
    TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
    TCP: Hash tables configured (established 65536 bind 65536)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp tru omap-iommu.1: sys registered
    highmem bounce pool size: 64 pages
    JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    msgmni has been set to 704
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    console [ttyO0] enabled
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_ua481aa000 (irq = 46) is a OMAP UART5
    brd: module loaded
    loop: module loaded
    ahci ahci.0: forcing PORTS_IMPL to 0x1
    ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst 
    scsi0 : ahci_platform
    ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
    odavinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
    CAN device driver interface
    CAN bus driver for Bosch D_CAN controller 1.0
    d_can d_can: d_can device registered (irq=52, irq_obj=53)
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    usbcore: registered new interface driver cdc_acm
    cdand ISDN adapters
    Initializing USB Mass Stomice: PS/2 mouse device common for all mice
    usb 2-1: new low speed USB device using musb-hdrc and address 2
    usb 2-1: New USB device fou
    usb 2-1: New USB devoduct=2, SerialNumberOM
    ta1: SATA lqt602240_ts 1-004a: Family ID: 128 Variant ID: 1 Version: 22 Build: 171
    qt602240_ts 1-004a: Matrix X Size: 18 Matrix Y Size: 12 Object Num: 17
    input: AT42QT602240/ATMXT224 Touchscreen as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/input/input0
    omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    i2c /dev entries driver
    Linux video capture interface: v2.00
    usbcore: registered new interface driver uvcvideo
    USB:04F3:0234.0001: input: USB HID v1.11 Mouse [OM] on usb-musb-hdrc.1-1/input0
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbf900000
    usbcore: registered new interface driver snd-usb-audio
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    ALSA device list:
      #0: TI81XX EVM
    nf_conntrack version 0.5.0 (9958 buckets, 39832 max)
    ip_tre Team
    TCP cubic registered
    NET: Registered protocol family 17
    can: controller area network core (rev 20090105 abi 8)
    NET: Registered protocol family 29
    can: raw protcan: broadcast manager protocol (rev 20090105 t)
    Registering the dns_resolver key type
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    Power Management for TI81XX.
    Detected MACID=40:5f:c2omap_rtc omap_rtc: setting system clmmc0: new high speed SDHC card at address aaaa
    mmcblk0: mmc0:aaaa SU08G 7.40 GiB 
     mmcblk0: p1 p2
    XT3-fs: barriers not enabled
    kinterval 5 seconds
    using internal journal recovery complete
    XT3-fs (mmcblk0p2 with writeback data mode
    VFS: Mounted root (ext3 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing init memory: 212K
    
    INIT: version 2.86 booting
    
    Ery
    PlStarting udev
    udevd (77): /proc/77/oom_adj is deprecated, please use /proc/77/oom_semounting rootaching udev devnodes
    NLSA: Restoring mixer seNo state is present for card EVM
    Found hardware: "" "" "" "" ""
    Hardware is initialized using a generic method
    No state is present for card EVM
    Configuring network interfaces... 
     : 0x4dd074
    : 0x4dd074
    AF(NETDEV_UP): eteth0      no wireless extensions.
    
    udhcpc (v1.13.2) started
    Sending discover...
    PHY: 0:01 - Link is Up RCONF(NETDEV_CHANGE): eth0: link becomes ready
    PSelect for 192.16ease of 192.168.0.117 obtained, lease time 86400
    adding dns 192.168.0.1
    done.
    Setting up IP spoofing protection: rp_filter.
    Mon Dec 31 10:37:00 UTC 2012
    Loading HDVICP2 Firmware
    DM814X prcm_config_app version: 2.0.0.1
    Doing PRCM settings...
    	PRCM for IVHD0 is in Progress, Please wait.....  
    			BW Phy Addr : 0x48180600 Data : 0x00000001
    			AW Phy Addr : 0x48180600 Data : 0x00000002
    			Phy Addr : 0x48180c04 Data : 0x000 0x48180620 Data : 0x00070000
    			AW Phy Addr : 0x48180620 Data : 0x00050002
    			BW Phy AddW Phy Addr : 0x48180c10 Data : 0x00000007
    			AW Phy Addr : 0x48180c10 Data : 0x00000003
    			Phy Addr : 0x48180c14 Data : 0x00000004
    			BW Phy Addr : 0x58088000 Data : 0xeafffffe
    			AW Phy Addr : 0x58088000 Data : 0xeafffffe
    			BW Phy Addr : 0x58098000 Data : 0xeafffffe
    			AW Phy Addr : 0x58098000 Data : 0xeafffffe
    			BW Phy Addr : 0x48180c10 Data : 0x00000003
    			AW Phy Addr : 0x48180c10 Data : 0x00000000
    			Phy Addr : CM for IVHD0 is Done S 
    ysLink version : 2.20.02eated on Date:Dec 26 2012 Time:18:39:49
    FIRMWARE: I2cInit will be done by M3
    FIRMWARE: Memory map bin file not passed
    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
    ===Mandatory arguments=== 
    <Processor Id>         0: DSP, 1: Video-M3, 2: Vpss-M3 
    <Location of Firmware> firmware binary file 
    <start|stop>           to start/stop the firmware 
    ===Optional arguments=== 
    -mmap                  input memory map bin file name 
    -i2c   efault memor
    Firmware Loader debefault FL_DEBUG: warninels: error, warning, info, debug, log
    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.2.1
    FIRMWARE: 1 start Successful
    Loading HDVPSS Firmware
    FIRMWARE: I2cInit will be done by M3
    FIRMWARE: Memory map bin file not passed
    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap 3 
    <Location of Firmware> firmware binary file 
    <start                input memory map bin file name 
    -i2c                   0: i2c init not done by M3, 1(default): i2c init done by M3 
    FIRMWARE: isI2cInitRequiredOnM3: 1
    FIRMWARE: Default memory configuration is used
    Firmware Loader debugging not configured
    Default FL_DEBUG: warning
    Allowed FL_DEBUG levels: error, warning, info, debug, log
    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.2.1
    FIRMWARE: 2 start Successful
    Configuring fb0 to LCD
    Hpec version 1.2
    2C No Ack
    
    
    tarting system message bus: dbus.
    Sdtarting telnet .
    Starting network benchmark server: netserver.
    Starting syslogd/klogd: .
    Sdev/memd at address 0x402c6000.
    Read at address  0x4dress 0x48180F04 (0x402c6f04): 0/mem opened.
    Memory mapped at address 0x40309000.
    Read at address  0x48180900 (0x40309900): 0x00000102
    Write at address 0x48180900 (0x40309900): 0x00000002, readback 0x00000002
    /dev/mem opened.
    Memory mapped at address 0x400f8000.
    Read at address  0x48180920 (0x400f8920): 0x00040002
    Write at address 0x48180920 (0x400f8920): 0x00000002, readback 0x00000002
    S.
    
            _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org dm814x-evm ttyO0
    
    Arago 2011.09 dm814x-evm ttyO0
    
    dm814x-evm login: oo  root
    
    
    Login incorrect
    
    lrPassword: 
    
    Login incorrect
    
    login: oot  Password: 
    Llogin: rotLogin timed out after 60 seconds
    
    _____  _           _         ___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org dm814x-evm ttyO0
    
    Arago 2011.09 dm814x-evm ttyO0
    
    dm814x-evm login: rot ot
    Password: 
    Login incorrect
    
    login: oo
    root@dm814x-evm:~# 
    
    root@dm814x-evm:~# 
    root@dm814x-evm:~# oot

    Yoel

  • Hello,

    Yoel Cohen said:
    how can I install ftp server in the EVM.

    TI has no ftp server on the EVM but you could check here and try it:

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/245038.aspx

    Best Regards,

    Margarita

  • Hello,

    Yoel Cohen said:
    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.04.22 15:26:15 =~=~=~=~=~=~=~=~=~=~=~=
    ge U-Boot will now be auto-loaded
    Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed
    Hit any key to stop autoboot:  0 
    reading u-boot.bin
    
    210400 bytes read
    ## Starting application at 0x80800000 ...
    
    
    U-Boot 2010.06 (Dec 26 2012 - 18:12:01)
    
    TI8148-GP rev 2.1
    
    ARM clk: 600MHz
    DDR clk: 400MHz
    
    I2C:   ready
    DRAM:  2 GiB
    NAND:  HW ECC BCH8 Selected
    No NAND device found!!!
    0 MiB
    MMC:   OMAP SD/MMC: 0
    *** Warning - bad CRC or NAND, using default env                          .:;rrr;;.                   
                        ,5#@@@@#####@@@@@@#2,             
                     ,A@@@hi;;;r5;;;;r;rrSG@@@A,          
                   r@@#i;:;s222hG;rrsrrrrrr;ri#@@r        
                 :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@:      
                B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B     
               @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@    
              @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@   
             @@;;rrsrrs@MB#@@@@@###@    @#;rsrsrsrsrr;r2ir @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@
           @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@
           @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@
           M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@#
           :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@,
            @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@ 
             @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@  
             ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@;  
              r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r   
               ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@,rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H      
             
                    .A@@         ;&@@@@MhXS5i5S                       :ihM#@@@@@##hs,                
    
    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:40:5f:c2:3e:7:93
    cpsw
    Hit any key to stop autoboot:  3  1 reading boot.scr
    
    354 bytes read
    Running bootscript from MMC/SD to set the ENV...
    
    151674 bytes read
    reading uImage
    age Name:   Arago/2.6.37-Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2796380 Bytes = 2.7 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... arting kernel ...
    
     Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Wed Dec 26 18:11:35 IST 2012
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing : 0xf000
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 160648
    Kernel command line: console=ttyO0,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M  notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 364MB 270MB = 634MB total
    Memory: 637324k/637324k available,  - 0xf8000000   ( 528 MB)
        lowmem  : 0xc0000000 - 0xd6c00000   ( 364 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .init : 0xc0008000 - 0xc003d000   ( 212 kB)
          .tex49000   (5168 kB)
          .data : 0xc054a000 - 0xc05970c0   ( 309 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC apts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ400
    Trying to install interrupt handler for IRQ401
    Trying to install interrupt handler for IRQ402
    Trying to install interrupt handler for IRQ403
    404
    Trying to install interrupt handler for IRQ405
    Trying to install interrupt 
    Trying to install type control for IRQ407
    Trying to set irq flags for IRQ407
    0000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buge driver init not yet happened.Faulting!
    omap_voltage_add_dev: VDD specified does not exist!
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core,request GPMC CS
    Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now
    registered ti81xx_vpss device
    registered ti81xx_vidout device
    registered ti81xx on-chip HDMI device
    registered ti81xx_fb device
    registered ti81xx_vin device
    ti81xx_pcie: Invoking PCI BIOS...
    ti81xx_pcie: Setting up Host Controller...
    ti81xx_pcie: Register base mapped @0xd7020000
    ti81xx_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers enabled
    bio: create slab <bio-0> atSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    USBSS revision 4ea2080b
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    pcf857x 1-0021: gpios 128..143 on a pcf8575
    regulator: VRTC: 1800 mV 
    regulator: VIO: 1500 mV 
    regulator: VDD1: 600 <--> 1500 mV at 1200 mV 
    regulator: VDD2: 600 <--> 1500 mV at 1200 mV 
    regulator: VDDCT3300 mV at 1800 mV 
    regulator: LDO3: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO4: 11: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO6: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO7: 1100 <--> 3300 mV at 3300 mV 
    regulator: LDO8: 1100 <--> 3300 mV at 1800 mV 
    tps65910 1-002d: No interrupt support, no core IRQ
    omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, host, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    MUSB controller-0 revision 4ea20800
    musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: SB HDRC host driver
    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb1: SerialNumber: musb-hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port db-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18
    musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    MUSB controller-1 revision 4ea20800
    musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: l family 2
    IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
    TCP established hash table entries: 65536 (order: 7, 524288 bytes)
    TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
    TCP: Hash tables configured (established 65536 bind 65536)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp tru omap-iommu.1: sys registered
    highmem bounce pool size: 64 pages
    JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    msgmni has been set to 704
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    console [ttyO0] enabled
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_ua481aa000 (irq = 46) is a OMAP UART5
    brd: module loaded
    loop: module loaded
    ahci ahci.0: forcing PORTS_IMPL to 0x1
    ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst 
    scsi0 : ahci_platform
    ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
    odavinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
    CAN device driver interface
    CAN bus driver for Bosch D_CAN controller 1.0
    d_can d_can: d_can device registered (irq=52, irq_obj=53)
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    usbcore: registered new interface driver cdc_acm
    cdand ISDN adapters
    Initializing USB Mass Stomice: PS/2 mouse device common for all mice
    usb 2-1: new low speed USB device using musb-hdrc and address 2
    usb 2-1: New USB device fou
    usb 2-1: New USB devoduct=2, SerialNumberOM
    ta1: SATA lqt602240_ts 1-004a: Family ID: 128 Variant ID: 1 Version: 22 Build: 171
    qt602240_ts 1-004a: Matrix X Size: 18 Matrix Y Size: 12 Object Num: 17
    input: AT42QT602240/ATMXT224 Touchscreen as /devices/platform/omap/omap_i2c.1/i2c-1/1-004a/input/input0
    omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    i2c /dev entries driver
    Linux video capture interface: v2.00
    usbcore: registered new interface driver uvcvideo
    USB:04F3:0234.0001: input: USB HID v1.11 Mouse [OM] on usb-musb-hdrc.1-1/input0
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbf900000
    usbcore: registered new interface driver snd-usb-audio
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    ALSA device list:
      #0: TI81XX EVM
    nf_conntrack version 0.5.0 (9958 buckets, 39832 max)
    ip_tre Team
    TCP cubic registered
    NET: Registered protocol family 17
    can: controller area network core (rev 20090105 abi 8)
    NET: Registered protocol family 29
    can: raw protcan: broadcast manager protocol (rev 20090105 t)
    Registering the dns_resolver key type
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    Power Management for TI81XX.
    Detected MACID=40:5f:c2omap_rtc omap_rtc: setting system clmmc0: new high speed SDHC card at address aaaa
    mmcblk0: mmc0:aaaa SU08G 7.40 GiB 
     mmcblk0: p1 p2
    XT3-fs: barriers not enabled
    kinterval 5 seconds
    using internal journal recovery complete
    XT3-fs (mmcblk0p2 with writeback data mode
    VFS: Mounted root (ext3 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing init memory: 212K
    
    INIT: version 2.86 booting
    
    Ery
    PlStarting udev
    udevd (77): /proc/77/oom_adj is deprecated, please use /proc/77/oom_semounting rootaching udev devnodes
    NLSA: Restoring mixer seNo state is present for card EVM
    Found hardware: "" "" "" "" ""
    Hardware is initialized using a generic method
    No state is present for card EVM
    Configuring network interfaces... 
     : 0x4dd074
    : 0x4dd074
    AF(NETDEV_UP): eteth0      no wireless extensions.
    
    udhcpc (v1.13.2) started
    Sending discover...
    PHY: 0:01 - Link is Up RCONF(NETDEV_CHANGE): eth0: link becomes ready
    PSelect for 192.16ease of 192.168.0.117 obtained, lease time 86400
    adding dns 192.168.0.1
    done.
    Setting up IP spoofing protection: rp_filter.
    Mon Dec 31 10:37:00 UTC 2012
    Loading HDVICP2 Firmware
    DM814X prcm_config_app version: 2.0.0.1
    Doing PRCM settings...
    	PRCM for IVHD0 is in Progress, Please wait.....  
    			BW Phy Addr : 0x48180600 Data : 0x00000001
    			AW Phy Addr : 0x48180600 Data : 0x00000002
    			Phy Addr : 0x48180c04 Data : 0x000 0x48180620 Data : 0x00070000
    			AW Phy Addr : 0x48180620 Data : 0x00050002
    			BW Phy AddW Phy Addr : 0x48180c10 Data : 0x00000007
    			AW Phy Addr : 0x48180c10 Data : 0x00000003
    			Phy Addr : 0x48180c14 Data : 0x00000004
    			BW Phy Addr : 0x58088000 Data : 0xeafffffe
    			AW Phy Addr : 0x58088000 Data : 0xeafffffe
    			BW Phy Addr : 0x58098000 Data : 0xeafffffe
    			AW Phy Addr : 0x58098000 Data : 0xeafffffe
    			BW Phy Addr : 0x48180c10 Data : 0x00000003
    			AW Phy Addr : 0x48180c10 Data : 0x00000000
    			Phy Addr : CM for IVHD0 is Done S 
    ysLink version : 2.20.02eated on Date:Dec 26 2012 Time:18:39:49
    FIRMWARE: I2cInit will be done by M3
    FIRMWARE: Memory map bin file not passed
    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
    ===Mandatory arguments=== 
    <Processor Id>         0: DSP, 1: Video-M3, 2: Vpss-M3 
    <Location of Firmware> firmware binary file 
    <start|stop>           to start/stop the firmware 
    ===Optional arguments=== 
    -mmap                  input memory map bin file name 
    -i2c   efault memor
    Firmware Loader debefault FL_DEBUG: warninels: error, warning, info, debug, log
    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.2.1
    FIRMWARE: 1 start Successful
    Loading HDVPSS Firmware
    FIRMWARE: I2cInit will be done by M3
    FIRMWARE: Memory map bin file not passed
    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap 3 
    <Location of Firmware> firmware binary file 
    <start                input memory map bin file name 
    -i2c                   0: i2c init not done by M3, 1(default): i2c init done by M3 
    FIRMWARE: isI2cInitRequiredOnM3: 1
    FIRMWARE: Default memory configuration is used
    Firmware Loader debugging not configured
    Default FL_DEBUG: warning
    Allowed FL_DEBUG levels: error, warning, info, debug, log
    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.2.1
    FIRMWARE: 2 start Successful
    Configuring fb0 to LCD
    Hpec version 1.2
    2C No Ack
    
    
    tarting system message bus: dbus.
    Sdtarting telnet .
    Starting network benchmark server: netserver.
    Starting syslogd/klogd: .
    Sdev/memd at address 0x402c6000.
    Read at address  0x4dress 0x48180F04 (0x402c6f04): 0/mem opened.
    Memory mapped at address 0x40309000.
    Read at address  0x48180900 (0x40309900): 0x00000102
    Write at address 0x48180900 (0x40309900): 0x00000002, readback 0x00000002
    /dev/mem opened.
    Memory mapped at address 0x400f8000.
    Read at address  0x48180920 (0x400f8920): 0x00040002
    Write at address 0x48180920 (0x400f8920): 0x00000002, readback 0x00000002
    S.
    
            _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org dm814x-evm ttyO0
    
    Arago 2011.09 dm814x-evm ttyO0
    
    dm814x-evm login: oo  root
    
    
    Login incorrect
    
    lrPassword: 
    
    Login incorrect
    
    login: oot  Password: 
    Llogin: rotLogin timed out after 60 seconds
    
    _____  _           _         ___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org dm814x-evm ttyO0
    
    Arago 2011.09 dm814x-evm ttyO0
    
    dm814x-evm login: rot ot
    Password: 
    Login incorrect
    
    login: oo
    root@dm814x-evm:~# 
    
    root@dm814x-evm:~# 
    root@dm814x-evm:~# oot

    I do not understand what is the question here.

    Best Regards,

    Margarita