We want to use Am335x with ONLY ONE (due to space constraint) 16 bits 4Gbit chip (512 Mb)
I read some answers from this forum about DDR3 using and have some doubts about it.
For example, some wrote that is max supported chip for DDRAM using 2Gbit , what creates some
doubts to me. I personaly didn't find this information in TI documents.
Also Starter Kit is built around 2Gb (256MB), not 4Gbit chip? I don't know if this concerns this restriction
or simple maybe 4Gbit chip wasn't available in this time.
It is strange that MAX total supported memory is 1GB and is possible use only one 16 bits Chip ?
It doesn't make any sense if it is true that is max allowed chip 2Gb.
To conclude: Could I get answer if possible use Am335X with ONLY ONE DDRAM3 4Gbit (X16) chip to have 512Mb memory ?
Thank in advance