Hi,
I am using IPNC 5.0, I have enabled AV server debugging
Below is my debug log,
./av_server.out DM365 NTSC APPRO2A AEWB 720P MPEG4 4000000 VBR AUTO MENUOFF &
AVSERVER API: Sending START.
AVSERVER MAIN: Recevied CMD = 0x0400, state = 0x0000
AVSERVER MAIN: AVSERVER_tskConnectInit() ...
AVSERVER MAIN: Create captureTsk ...
CAPTURE: Recevied CMD = 0x0300
CAPTURE: Create...
CAPTURE: Opening capture on imager MICRON_MT9P031_5MP.
SENSOR FPS VALUE = 30
CAPTURE: Create...DONE
AVSERVER MAIN: Create encodeTsk ...
AVSERVER MAIN: Create streamTsk ...
STREAM: Recevied CMD = 0x0300
STREAM: Create...
STREAM: Ext 0: 0x0
STREAM: Ext 1: 0x0
queue id:131076
STREAM: Create...DONE
AVSERVER MAIN: Create fdTsk ...
FR : 0 users registered from exsiting face album
AVSERVER MAIN: Create displayTsk ...
AVSERVER MAIN: Create aewbTsk ...
IPNC_DM365_5.0.0 (root@ubuntu) (gcc version 4.3.3 (GCC) ) #1 PREEMPT Mon Apr 2
IPNC AUTO_IRIS = 1
AVSERVER MAIN: Create audioPlayTsk ...
AVSERVER MAIN: Create motionTsk ...
AVSERVER MAIN: Create swosdTsk ...
AVSERVER MAIN: Allocing Buffers ...
AVSERVER MAIN: Allocating buffers ...
AVSERVER MAIN: Stream 0: Allocating LDC buffers: 0 of size 1413248 bytes
AVSERVER MAIN: Stream 0: Allocating VNF buffers: 0 of size 1413248 bytes
AVSERVER MAIN: Stream 0: Allocating Encode IN buffers: 3 of size 1413248 bytes
AVSERVER MAIN: Stream 0: Assigning Resize IN buffers: 0 of size 1413248 bytes
AVSERVER MAIN: Stream 0: Getting Capture OUT buffers
AVSERVER MAIN: Stream 0: Capture OUT buffers 0
AVSERVER MAIN: Stream 0: Capture OUT buffers 1
AVSERVER MAIN: Stream 0: Capture OUT buffers 2
AVSERVER MAIN: Stream 1: Allocating LDC buffers: 0 of size 92288 bytes
AVSERVER MAIN: Stream 1: Allocating VNF buffers: 0 of size 92288 bytes
AVSERVER MAIN: Stream 1: Allocating Encode IN buffers: 3 of size 92288 bytes
AVSERVER MAIN: Stream 1: Assigning Resize IN buffers: 0 of size 92288 bytes
AVSERVER MAIN: Stream 1: Getting Capture OUT buffers
AVSERVER MAIN: Stream 1: Capture OUT buffers 0
AVSERVER MAIN: Stream 1: Capture OUT buffers 1
AVSERVER MAIN: Stream 1: Capture OUT buffers 2
As displayed in debug log it is showing two streams. stream 0 and stream 1. Why two streams needed? Is it really required or its bug?