This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel debugging the DSP application in omapl138

Other Parts Discussed in Thread: OMAPL138

Hi,

 I am using OMAPL138,here ARM boots the DSP via DSPLINK .When i try to connect the Jtag XDS100V2 usb emulator to debug the dsp application in CCS V5 i got the error as 

    error connecting to the target: (error -2131 @ 0x0) unable to access device register. reset the device, and retry the operation. if error persists, confirm configuration, power-cycle the board, and/or try more reliable jtag settings (e.g. lower tclk). (emulation package 5.0.520.0)

It will be more helpful if i could do parallel debugging.please help me

  • Hi Malini,

    Few questions/suggestions here,

    1. Whether it is a custom board which uses OMAPL138 or OMAPL138 EVM or OMAPL138 LCDK ?

    2. Make sure you use the appropriate GEL file and CCXML configuration file. Have you done the "test connection" with the target  after configuring CCXML?

    3. Have a look at " Debugging JTAG Connectivity Problems"

    Regards,

    Shankari

    --------------------------------------------------------------------------------------------------------
    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------