This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where to get MsgRouter binary which is part of TI syslib?

Hi, I am a TI 6614 evm user, after installation of TI's ccs and sc-mcsdk package, I did not find any MsgRouter.out binary in syslib folder under TI's installation path.

From the TI's documentation it seems that MsgRouter is one of  prerequisites to use inter-processor messaging.

The strange thing is the syslib seems to be installed successfully after install sc-mcsd pkg, as we could find source&lib like MsgCom, Agent, .etc,. under syslib folder.

The CCS version is: CCS5.1.1.00033_linux;

The sc-mcsdk version is : sc_mcsdk_2_00_00_09_setuplinux;

Any one could help?

  • Hello!

    The msgrouter.out file should be found under sc_mcsdk_linux_x_xx_xx_xx --> linux-devkit --> arago-xxxx.xx --> armv7a --> arm-none-linux-gnueabi --> usr --> bin.  My sc_mcsdk version is not the same as yours but I believe the path should be consistent/close.  If it's not there, try doing a search over the entire sc_mcsdk directory.

    Also, 6614 is not a device supported on the public e2e forums.  For future support, please contact your local FAE or similar support system.

    -John Demery