This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting a serial dot matrix display to OMAP L138



Hi,

Is there any efficient way to connect a serial 5x7 AlphaNumeric Display to the L138 or do I have to use GPIO?

I was thinking of a display from AVAGO - HCMS3901

Pin Function Description:

RESET (RST) -  Sets Control Register bits to logic low. The Dot Register contents are unaffected by the
Reset pin. (logic low = reset; logic high = normal operation).

DATA IN (DIN) - Serial Data input for Dot or Control Register data. Data is entered on the rising edge of the Clock input.


DATA OUT (DOUT) - Serial Data output for Dot or Control Register data. This pin is used for cascading multiple displays
.
CLOCK (CLK) - Clock input for writing Dot or Control Register data. When Chip Enable is logic low, data is entered on the rising Clock edge.

REGISTER SELECT (RS) - Selects Dot Register (RS = logic low) or Control Register (RS = logic high) as the
destination for serial data entry. The logic level of RS is latched on the falling edge of the Chip Enable input.

CHIP ENABLE (CE) - This input must be a logic low to write data to the display. When CE returns to logic
high and CLK is logic low, data is latched to either the LED output drivers or a Control Register.

OSCILLATOR SELECT - Selects either an internal or external display oscillator source. (SEL) (logic low = External
Display Oscillator; logic high = Internal Display Oscillator).


OSCILLATOR (OSC) - Output for the Internal Display Oscillator (SEL = logic high) or input for an External
Display Oscillator (SEL = logic low).

Thanks a lot,

Yu6622.AV02-0868EN,0 VVVVV.pdf