Hello,
I am trying to connect to a C6678 evaluation board via JTAG and I’m getting the following error:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.0.747.0)
I haven’t had this problem in the past. The only difference is that I’m now using rev.3 of the board. Has anyone ever seen this issue?
Thanks,
Sachan