hi,dear friends:
Recently,I found a docment ---Previewer-Resizer_Driver_SDS_C. Inside it said that IPIPE input buffer
addresses must be multiple of 32.But what did that word ----- "IPIPE input buffer addresses must be
multiple of 32" mean?
It mean that height and width of image VPFE captured must be mutiple of 32
if my guess was right, why can we capture resolution of 1920x1080 ,Inside that 1080 was be divided
with remainder(1080/32 = 33.75) . the other side ,I also heard that when you want to capture 1600x1200 ,
you must capture 1600x1216 .Because 1200 was divided with remainder, but 1216 not.
which one was right ?