Dear All,
I have certain Douts Regardig Mounting of Resistor and Capacitor of DSP0_DDR3_ECKP_0, The Resistor R37,R38 & Capacitor C31 from schematic of EVM.
In the Evaluation board there there are certain resistors and capacitors are mounted near the DDR3 Chip.
The DSP0_DDR3_ECKP_0 is connected to R37,R38 & C31 . I have also attached the schematic of the EVM i am refering. With Reference to the Page No.13
Whether the R37,R38 & C31 should mount near the DDR3 Chip?
Suppose if the DDR3 Chip and the processor are mounted on top of the board and the R37,R38 & C31 are mounted on bottom of the board. Will it cause any issue?
Regards,
Avinash N