This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Transfer of uImage from TFTP server fails with the RAM address mentioned in SPI flashing procedure.



I use the following link to set up kernel booting from SPI flash :

http://processors.wiki.ti.com/index.php/Booting_Linux_kernel_using_U-Boot

However, I am stuck at the point :

U-Boot> tftp 0xc0700000 uImage

Following is the screen shot of TeraTerm window :

BARCO_UBOOT#tftp 0xc0700000 uImage
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 10.64.16.174; our IP address is 10.64.16.63
Filename 'uImage'.
Load address: 0xc0700000
Loading: #

Last, but not the least, I need to know the exact value of offsets for flashing uImage & filesystem to the flash (Winbond 4096 KiB W25X32 SPI chip) used in DM8148 EVM(Mistral).