This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure OMX and DSP application on DM8168 and EZSDK 5.05.02.00



Hello

i am tring to run DSP codec engine examples on DSP on DM8168. I found some problems when i run at the same time capture_encode and universal_copy. I read the following forums:

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/149505.aspx

I use the default memory map from http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map. I modified the files:

1)  remote.cfg in apps/universal_copy

//Processor.heapId = common.MessageQ_heapMap["Ipc"];
//Processor.sharedRegionId = common.SharedRegion_map["Ipc"];
Processor.heapId = 0;  //  <-- Don't know why
Processor.sharedRegionId = common.SharedRegion_map["SysLink: HOST<--->DSP"];

2) serverplatforms.xs in servers/all_codecs

var TI816X_DSP_ExtMemMap = {
/*
            DDR3_HOST: {
                comment: "DDR3 Memory reserved for use by the A8",
                name: "DDR3_HOST",
                base: 0x80000000,
                len:  0x0B000000    // 176 MB
            },
            DDR3_DSP: {
                comment: "DDR3 Memory reserved for use by the C674",
                name: "DDR3_DSP",
                base: 0x8B000000,
                len:  0x01800000    // 24 MB
            },
            DDRALGHEAP: {
                comment: "DDR3 Memory reserved for use by algorithms on the C674",
                name: "DDRALGHEAP",
                base: 0x8C800000,
                len:  0x00800000    // 8 MB
            },
            DDR3_SR1: {
                comment: "DDR3 Memory reserved for use by SharedRegion 1",
                name: "DDR3_SR1",
                base: 0x8D000000,
                len:  0x00C00000    // 12 MB
            },
            DDR3_HDVPSS: {
                comment: "DDR3 Memory reserved for use by HDVPSS",
                name: "DDR3_HDVPSS",
                base: 0x8DC00000,
                len:  0x00200000    // 2 MB
            },
            DDR3_V4L2: {
                comment: "DDR3 Memory reserved for use by V4L2",
                name: "DDR3_V4L2",
                base: 0x8DE00000,
                len:  0x00200000    // 2 MB
            },
            DDR3_SR0: {
                comment: "DDR3 Memory reserved for use by SharedRegion 0",
                name: "DDR3_SR0",
                base: 0x8E000000,
                len:  0x01000000    // 16 MB
            },
            DDR3_M3: {
                comment: "DDR3 Memory reserved for use by the M3 core",
                name: "DDR3_M3",
                base: 0x8F000000,
                len:  0x01000000    // 16 MB
            },*/
     DDR3_DSP: {
         comment: "DDR3 Memory reserved for use by the C674",
         name: "DDR3_DSP",
         base: 0x99500000,
         len: 0xc00000 /* 12 MB (Default memory reserved for c674x changed based on size of the DSP code)*/
         },
     DDRALGHEAP: {
         comment: "DDR3 Memory reserved for use by algorithms on the C674",
         name: "DDRALGHEAP",
         base: 0x98000000,
         len: 0x00400000 /* 4 MB (Region used by algs and codec engine for memory allocations) */
         },
     DDR3_SR1: {
         comment: "DDR3 Memory reserved for use by SharedRegion 1 (IPC)",
         name: "DDR3_SR1",
         base: 0x99400000,
         len: 0x00100000 /* 1 MB */
         },
     DDR3_SR0: {
         comment: "DDR3 Memory reserved for use by SharedRegion 0 (SYSLINK)",
         name: "DDR3_SR0",
         base: 0x9F700000,
         len: 0x00200000 /* 2 MB */
 },
};

3) remote.cfg in buidutils

    /* first set module defaults ... */
    //Processor.heapId = common.MessageQ_heapMap["Ipc"];
    //Processor.sharedRegionId = common.SharedRegion_map["Ipc"];
    Processor.heapId = 0;  //  <-- Don't know why
    Processor.sharedRegionId = common.SharedRegion_map["SysLink: HOST<--->DSP"];

    /* ... then add per-processor settings */
    var coreComm = {};
    coreComm.numMsgs = 64;
    coreComm.msgSize = 4 * 1024;
    coreComm.heapId = Processor.heapId;
    coreComm.userCreatedHeap = false;
    coreComm.sharedRegionId = Processor.sharedRegionId;
    if (platform.match("TI814X") || platform.match("TI816X") ||
            platform.match("DM8148") || platform.match("DM8168")) {
        Processor.coreComm.$add(coreComm);
        Processor.coreComm.$add(coreComm);
        //Processor.coreComm.$add(coreComm);
        //Processor.coreComm.$add(coreComm);
    }

4) ti_platforms_evmTI816x.cfg in servers/all_codecs

/*
var entry2 = new SharedRegion.Entry();

entry2.base = ipcSharedMem.base;
entry2.len = ipcSharedMem.len;
entry2.ownerProcId = MultiProc.getIdMeta("HOST");
entry2.isValid = true;
entry2.createHeap = true;
entry2.cacheEnable = true;
entry2.name = "IpcShared";

SharedRegion.setEntryMeta(
    common.SharedRegion_map["Ipc"],  
    entry2
);*/

5) The load script configuration is this:


        echo "Loading PRCM & SYSLINK"
    prcm_config_app s
        modprobe syslink
        until [[ -e /dev/syslinkipc_ProcMgr && -e /dev/syslinkipc_ClientNotifyMgr ]]
        do                                                
            sleep 0.5
        done

    echo "Loading CMEM for C674 Firmware"
    modprobe cmemk phys_start=0x96C00000 phys_end=0x97ffffff pools=20x4096,10x131072,2x1048576

    echo "Loading HDVICP2 Firmware"
    firmware_loader $HDVICP2_ID /usr/share/ti/ti-media-controller-utils/dm816xbm_m3video_whole_program_debug.xem3 start -mmap /usr/share/ti/ti-media-controller-utils/mm_dm81xxbm_vc3.bin -i2c 0

        echo "Loading HDVPSS Firmware"
    firmware_loader $HDVPSS_ID /usr/share/ti/ti-media-controller-utils/dm816xbm_m3vpss_whole_program_debug.xem3 start -mmap /usr/share/ti/ti-media-controller-utils/mm_dm81xxbm_vc3.bin -i2c 0
 

Questions:

- If i set heapId=3 in remote.cfg (like the forum) the application does not start. If i set this value to 0 the application runs. Why? The application runs while capture_encode is running.

- Why in the forum i have to comment the 2 Processor.coreComm.$add(coreComm); ? What does this function do?

Problems:

When i run the universal application and the capture_encode is running there are no errors. When the capture_encode stop i can see this trace and the systems crashes.

 tearing down the capture-encode example
 exiting thread
 exiting thread
 exiting thread
 exiting thread
 got eventState changed to: OMX_StateIdle
 capture state idle
 got eventState changed to: OMX_StateIdle
 DEI state idle
 got eventState changed to: OMX_StateIdle
 display state idle
 got eventState changed to: OMX_StateIdle
 display control state idle
 got eventState changed to: OMX_StateIdle
 Encoder state idle
 got eventState changed to: OMX_StateLoaded
 display state loaded
 got eventState changed to: OMX_StateLoaded
 ctrl-dc state loaded
 got eventState changed to: OMX_StateLoaded
 encoder state loaded
 got eventState
Unable to handle kernel paging request at virtual address d6000008
changed to: OMX_pgd = c6cac000
StateLoaded
 d[d6000008] *pgd=00000000ei state loaded

 Deallocate buInternal error: Oops: 5 [#1]
last sysfs file: /sys/devices/platform/omap/omap_i2c.2/i2c-2/2-0010/resolution
Modules linked in: dma_mmap mt9m031 ti81xxvin ti81xxvo ti81xxfb vpss cmemk syslink ipv6
CPU: 0    Not tainted  (2.6.37+ #4)
PC is at HeapMemMP_free+0x1c8/0x400 [syslink]
LR is at GateMP_enter+0x80/0xa0 [syslink]
pc : [<bf099634>]    lr : [<bf094eb4>]    psr: 60000013
sp : c6435e60  ip : 00000000  fp : c6435e94
r10: 00151800  r9 : 00000000  r8 : bebf29d4
r7 : d6000008  r6 : d37e6000  r5 : d6000080  r4 : d6000000
r3 : 00000000  r2 : 00000000  r1 : 00060000  r0 : 00000000
Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
Control: 10c5387d  Table: 86cac019  DAC: 00000015
Process capture_encode_ (pid: 1333, stack limit = 0xc64342e8)
Stack: (0xc6435e60 to 0xc6436000)
5e60: d6000080 00151800 c6435e94 00000000 c01cf35a bebf29d4 0000000f bebf29d4
5e80: c6434000 00000000 c6435ef4 c6435e98 bf0cfe38 bf099478 c01cf35a bebf29d4
5ea0: 00000000 d37e3000 80000080 00151800 40138450 bebf2a1c 0010ee20 0000ac2c
5ec0: c6435eec a0000013 c6435ef4 c6435ed8 c01e5020 c0069cac c64459f0 00000000
5ee0: c6c4a880 0000000f c6435f04 c6435ef8 c00d3c34 bf0cfcac c6435f74 c6435f08
5f00: c00d4344 c00d3c18 40277000 c6421e00 c01e1ab0 c6677c40 50db1fee 33428f00
5f20: c00545c0 c6421e00 40277000 c6435f70 0000003c 40277000 c6434000 00000000
5f40: 00000001 0000003c 00000000 00000000 bebf29d4 c01cf35a 0000000f c6c4a880
5f60: c6434000 00000000 c6435fa4 c6435f78 c00d43dc c00d3e50 00000000 00000001
5f80: 50db1fee bebf29d4 c01cf35a 000f9518 00000036 c0046fa8 00000000 c6435fa8
5fa0: c0046e00 c00d4390 bebf29d4 c01cf35a 0000000f c01cf35a bebf29d4 00000001
5fc0: bebf29d4 c01cf35a 000f9518 00000036 00000000 00000000 4009b000 bebf2abc
5fe0: 000f952c bebf29a8 00086efc 40208aec 20000010 0000000f 00000000 00000000
Backtrace:
[<bf09946c>] (HeapMemMP_free+0x0/0x400 [syslink]) from [<bf0cfe38>] (HeapMemMPDrv_ioctl+0x198/0x77c [syslink])
[<bf0cfca0>] (HeapMemMPDrv_ioctl+0x0/0x77c [syslink]) from [<c00d3c34>] (vfs_ioctl+0x28/0x44)
 r6:0000000f r5:c6c4a880 r4:00000000
[<c00d3c0c>] (vfs_ioctl+0x0/0x44) from [<c00d4344>] (do_vfs_ioctl+0x500/0x540)
[<c00d3e44>] (do_vfs_ioctl+0x0/0x540) from [<c00d43dc>] (sys_ioctl+0x58/0x7c)
[<c00d4384>] (sys_ioctl+0x0/0x7c) from [<c0046e00>] (ret_fast_syscall+0x0/0x30)
 r8:c0046fa8 r7:00000036 r6:000f9518 r5:c01cf35a r4:bebf29d4
Code: e3a01008 e30f2fff e3a03001 ebff66a7 (e5940008)
ffers capture 0,---[ end trace 42c3b980df6544ae ]---
 ptr 0x44818080, size 1382400

Thanks for the help